Results 1 to 8 of 8

Thread: The Raspberry pi 4 Model B

Threaded View

Previous Post Previous Post   Next Post Next Post
  1. #1

    The Raspberry pi 4 Model B

    Well I have 2 of the new rpi4's with 4GB of Memory on pre-order. This will be nice.

    Raspberry Pi 4 specs

    • SoC: Broadcom BCM2711B0 quad-core A72 (ARMv8-A) 64-bit @ 1.5GHz
    • GPU: Broadcom VideoCore VI
    • Networking: 2.4 GHz and 5 GHz 802.11b/g/n/ac wireless LAN
    • RAM: 1GB, 2GB, or 4GB LPDDR4 SDRAM
    • Bluetooth: Bluetooth 5.0, Bluetooth Low Energy (BLE)
    • GPIO: 40-pin GPIO header, populated
    • Storage: microSD
    • Ports: 2 × micro-HDMI 2.0, 3.5 mm analogue audio-video jack, 2 × USB 2.0, 2 × USB 3.0, Gigabit Ethernet, Camera Serial Interface (CSI), Display Serial Interface (DSI)
    • Dimensions: 88 mm × 58 mm × 19.5 mm, 46 g
    Last edited by LloydF; 06-24-2019 at 10:54 AM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX 3D Model(s) for printing
    By r3n33 in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 09-03-2015, 03:56 PM
  2. gearbox 3d model
    By sthmck in forum Mech Warfare
    Replies: 1
    Last Post: 12-11-2014, 08:54 PM
  3. MX-64- which model of Maxon motors?
    By vinjk in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 07-21-2014, 04:59 AM
  4. 3D Model Thread?
    By YoMarchYo in forum Mech Warfare
    Replies: 0
    Last Post: 04-07-2013, 02:40 AM
  5. CAD Model of Phidgets
    By cmmguy in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 04-23-2008, 03:56 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •