Results 1 to 5 of 5

Thread: The Raspberry pi 4 Model B

  1. #1

    The Raspberry pi 4 Model B

    Well I have 2 of the new rpi4's with 4GB of Memory on pre-order. This will be nice.

    Raspberry Pi 4 specs

    • SoC: Broadcom BCM2711B0 quad-core A72 (ARMv8-A) 64-bit @ 1.5GHz
    • GPU: Broadcom VideoCore VI
    • Networking: 2.4 GHz and 5 GHz 802.11b/g/n/ac wireless LAN
    • RAM: 1GB, 2GB, or 4GB LPDDR4 SDRAM
    • Bluetooth: Bluetooth 5.0, Bluetooth Low Energy (BLE)
    • GPIO: 40-pin GPIO header, populated
    • Storage: microSD
    • Ports: 2 × micro-HDMI 2.0, 3.5 mm analogue audio-video jack, 2 × USB 2.0, 2 × USB 3.0, Gigabit Ethernet, Camera Serial Interface (CSI), Display Serial Interface (DSI)
    • Dimensions: 88 mm × 58 mm × 19.5 mm, 46 g
    Last edited by LloydF; 06-24-2019 at 10:54 AM.

  2. #2

    Re: The Raspberry pi 4 Model B

    Neat! Really glad they added Gigabit Ethernet.

    Are there any benchmarks on the VideoCore VI?

  3. #3

    Re: The Raspberry pi 4 Model B

    I got my first RPI4 today have the Raspberry Desktop running and am now working on ROS. Happy day's
    (Note. Tried a 1080p monitor, and this board runs way hot even with heat sinks in 4k with 3840 by 2160 or just 1080p.
    A fan is really needed here)
    Last edited by LloydF; 07-06-2019 at 12:33 PM.

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: The Raspberry pi 4 Model B

    In theory, the RPi4+4GB is more powerful than my netbook in its default configuration (2-core 1.0GHz/1.33GHz, 4GB, USB2, Fast Ethernet, 802.11n)...

    Probably will pick up one of the RPi4+4GB in the next month, or so, to see if I can get anything like my netbook performance with the RPi4 running off SD and/or USB3 thumbdrive.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  5. #5

    Re: The Raspberry pi 4 Model B

    If it is true that Walmart is going to carry the rpi4, this could be the pi's chance to really shine.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX 3D Model(s) for printing
    By r3n33 in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 09-03-2015, 03:56 PM
  2. gearbox 3d model
    By sthmck in forum Mech Warfare
    Replies: 1
    Last Post: 12-11-2014, 08:54 PM
  3. MX-64- which model of Maxon motors?
    By vinjk in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 07-21-2014, 04:59 AM
  4. 3D Model Thread?
    By YoMarchYo in forum Mech Warfare
    Replies: 0
    Last Post: 04-07-2013, 02:40 AM
  5. CAD Model of Phidgets
    By cmmguy in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 04-23-2008, 03:56 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •