Results 1 to 7 of 7

Thread: Project Khepri - MX 106 hexapod.

  1. #1
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    847
    Images
    25
    Rep Power
    85

    Project Khepri - MX 106 hexapod.

    Khepri is a self built AI platform for DNN exploration. It has an onboard Nvidia 1070GTX for processing. In a standing position it is one meter in diameter and weighs in at 13kg. The leg actuators are Dynamixel MX106s and MX64s in the coxa positions. All “shells” were modeled in Maya and printed by Shapeways on their SLS printers. Power is provided by a custom lithium ion battery. Voltage is regulated to computer, actuators and LEDs by voltage converters by MiniBox. Onboard CPU is an Intel i5, 16Gig of ram and 120Gig SSD. Running ROS and my own hexapod stack.


  2. #2

    Re: Project Khepri - MX 106 hexapod.

    Pretty Cool! Looks like you are having some fun!

  3. #3

    Re: Project Khepri - MX 106 hexapod.

    Very nice!

    I was thinking "can those nylon brackets really carry 5 kg each?" all the way until I saw they were just covers on top of the metal brackets :-)

    What do you use to interface with the Dynamixels from the mini-PC?

  4. #4
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    847
    Images
    25
    Rep Power
    85

    Re: Project Khepri - MX 106 hexapod.

    A U2D2 jwatte at 3Mbps. All the dynamixels are protocol 2.0 as well, so far I'm loving the extra features protocol 2 gives. Also the "mini-PC" is a Zotac VR box. It has a 1070GTX on board. Runs a bit warm but ventilation is working well.

  5. #5

    Re: Project Khepri - MX 106 hexapod.

    That's funny; my first walker was an all-MX-64 quad with a Zotac mini-box, too. But it was one of those earlier AMD APU ones, not worth the extra weight in the end.

    Have you trained any cool models for the GPU yet?

  6. #6
    Join Date
    Jun 2011
    Location
    USA
    Posts
    538
    Images
    107
    Rep Power
    39

    Re: Project Khepri - MX 106 hexapod.

    That's impressive! Nice work. Diving right into the fun stuff next, or doing more refinement first?

  7. #7
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    847
    Images
    25
    Rep Power
    85

    Re: Project Khepri - MX 106 hexapod.

    A little of both Gertlex. I'm trying to tackle the PID side of things at the moment. As well as getting TensorFlow integrated with my ROS stack.

Thread Information

Users Browsing this Thread

There are currently 3 users browsing this thread. (0 members and 3 guests)

Similar Threads

  1. Project ROS Hexapod project Golem: MX-64 4dof
    By KevinO in forum Project Showcase
    Replies: 147
    Last Post: 08-23-2016, 11:34 AM
  2. Project My next hexapod project, codename BMX
    By Zenta in forum Project Showcase
    Replies: 29
    Last Post: 01-12-2015, 02:05 PM
  3. Project ROS Hexapod project Golem: MX-64 4dof
    By KevinO in forum Humanoids, Walkers & Crawlers
    Replies: 63
    Last Post: 10-21-2014, 11:23 AM
  4. Hexapod Project
    By jcrazy in forum Robotics General Discussion
    Replies: 5
    Last Post: 05-04-2011, 10:49 PM
  5. Project Ally -My First Hexapod Project
    By parallax in forum Project Showcase
    Replies: 28
    Last Post: 07-17-2010, 04:30 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •