Results 1 to 6 of 6

Thread: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

  1. U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    Hi! This is my first 'technical' post in the Trossen Robotics Community forum. I am happy to be here. Especially because i need help! :-P

    Ok. I am building a mobile robotic plattform with 8 XM430-W350-R motors.

    I have 4 LIPO Battery 11.1V 1800mAh LB-012. I want use the U2D2 Power Hub to give power to the Dynamixel motors. However, i don't know how to connect the battery to the U2D2 Power Hub. Can anybody help me??

    Thanks in advance!

    JC

    LIPO Battery 11.1V 1800mAh LB-012

  2. #2
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    847
    Images
    25
    Rep Power
    85

    Re: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    It has three different power connectors on board. I'm not sure what you mean?


  3. Re: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    Yes, yes. Thank you for fast reply! I have this battery. How i connect the battery T-Connector to the 'U2D2 power hub' power connectors? In the pictures it seems totally incompatible....

    JC


  4. Re: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    Well.

    I don't know how to connect the LIPO Battery 11.1V 1800mhA LB-012 T-Connector to the U2D2 Power Hub Board power connectors. They seems incompatible. Do i need a adaptor cable or so?

    JC

  5. #5
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,282
    Images
    27
    Rep Power
    275

    Re: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    The problem is that battery uses a Deans / T-connector and the board does not have that anywhere on it. So, you need something like this (https://www.trossenrobotics.com/battery-wiring-harness) or build your own male Deans/T-connector to barrel connector or bare wires that must never leave the screw connector to prevent damage to the battery and/or accidentally apply reverse polarity to the servos.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  6. Re: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    Yes, tician. That was my problem. Thanks! Your answer was useful for me. You put me on the track.

    I found:

    Click image for larger version. 

Name:	539dccbaa506434a187bfb533ef376cc_1562923801_91.jpg 
Views:	10 
Size:	47.0 KB 
ID:	7571



    I think it would fit my needs. However now I have another problem. I will release another thread soon to describe it.

    JC

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) How often to recharge LIPO battery?
    By Snoopy in forum Power
    Replies: 8
    Last Post: 11-14-2017, 08:12 PM
  2. lipo battery for irobot
    By hazaza in forum Power
    Replies: 5
    Last Post: 04-18-2013, 08:00 PM
  3. Question(s) Max amp load on LiPo battery
    By alonso in forum Power
    Replies: 7
    Last Post: 04-06-2013, 01:42 AM
  4. Question(s) 4S 14.8v lipo battery is charging to 16.5v??
    By alonso in forum Power
    Replies: 2
    Last Post: 10-14-2012, 11:23 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •