I have recently started working with Dynamixel XM430-W350-R servo motors. In 'position mode' the motor offers an accuracy of 4096 points for a full 360º rotation (with an absolute encoder).
Therefore, in order to arrive at a specific position, a value between 0 and 4095 must be indicated. However, if for example I am at 1, and I want to get to "-1" (by the shortest route) I can not. Instead the servo motor should move up to 4095 making a turn of almost 360 degrees. I mean, it looks like zero ("0") can't be crossed. True?
My question is: Is it possible to "move" the zero position to an arbitrary position (by means of a calibration procedure, reset...)? How?
If it is not possible (!), what is the right approach?
Thanks!
JC
Bookmarks