Results 1 to 3 of 3

Thread: Absolute zero position for Dynamixel XM430-W350-R: How to change it?

  1. Question Absolute zero position for Dynamixel XM430-W350-R: How to change it?

    I have recently started working with Dynamixel XM430-W350-R servo motors. In 'position mode' the motor offers an accuracy of 4096 points for a full 360º rotation (with an absolute encoder).

    Therefore, in order to arrive at a specific position, a value between 0 and 4095 must be indicated. However, if for example I am at 1, and I want to get to "-1" (by the shortest route) I can not. Instead the servo motor should move up to 4095 making a turn of almost 360 degrees. I mean, it looks like zero ("0") can't be crossed. True?

    My question is: Is it possible to "move" the zero position to an arbitrary position (by means of a calibration procedure, reset...)? How?

    If it is not possible (!), what is the right approach?

    Thanks!

    JC
    Last edited by jcarlos; 08-04-2019 at 03:50 PM.

  2. #2

    Re: Absolute zero position for Dynamixel XM430-W350-R: How to change it?

    The documentation for Dynamixel protocol 2 (used by the XM430) talks about this. There is, for example, a "multi turn" mode. Or you can turn on "wheel mode," move forward, and then turn back on "joint mode." (That's what you had to do in the version 1 protocol, at least for certain versions)

    If you read through the protocol description, you will find the options they have for this case: http://emanual.robotis.com/docs/en/d...of-eeprom-area

  3. Re: Absolute zero position for Dynamixel XM430-W350-R: How to change it?

    Thank you so much for responding so quickly, jwatte . Yes, theses solutions you propose are feasible, but I don't really need more than 360 degrees. The Homing position parameter has turned out to be just what I was looking for.

    JC
    Last edited by jcarlos; 08-05-2019 at 10:19 AM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Power for eight (8) Dynamixel XM-430-W350-R
    By jcarlos in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 04-10-2021, 02:28 AM
  2. Question(s) Motor model for XM430-W350-R
    By kyrtoner2 in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 09-29-2018, 07:52 AM
  3. Question(s) Dynamixel XL/XM on WX250 Arm: Can't writeWord to Change Position, Velocity
    By JDS in forum Software and Programming
    Replies: 6
    Last Post: 09-19-2018, 08:49 PM
  4. Cannot connect to Dynamixel XM430-W210-T by USB2Dynamixel adapter
    By robomaniacpl in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 02-14-2018, 11:44 PM
  5. Dynamixel position accuracy, calibration
    By Adam in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 05-19-2010, 10:55 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •