Results 1 to 2 of 2

Thread: 4 Dof Hexapod Torque calculations

  1. 4 Dof Hexapod Torque calculations

    Hello all,

    I am currently off from college and I am trying to calculate the torque acting on a 4 DOF hexapod has anyone already done this or can help as I'm running in circles with it.

  2. #2

    Re: 4 Dof Hexapod Torque calculations

    Each joint can be individually calculated as if all the other joints are stiff, so I get pretty close by measuring the distance to the base points and the center of mass / weight of the body between the joint and that base point.

    For example, a joint that's right above a foot, actually should get no torque, just down-force, as long as the other joints are rigid.

    This isn't 100% accurate, though -- you really need a CAD package with 3D force/torque analysis to do that.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Using AX-12A in zero torque mode.
    By ZanQdo in forum DYNAMIXEL & Robot Actuators
    Replies: 9
    Last Post: 06-20-2015, 03:23 AM
  2. Matrix calculations
    By navidahmeduom in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 05-15-2015, 03:41 PM
  3. Question(s) Quadruped torque calculations - Confirmation Please!!!
    By Ferret in forum Humanoids, Walkers & Crawlers
    Replies: 25
    Last Post: 07-06-2013, 02:41 AM
  4. Servo torque required for hexapod
    By Fatfrank69 in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 02-19-2013, 05:08 PM
  5. Voltage Sensor calculations
    By super-d in forum Sensors
    Replies: 3
    Last Post: 03-01-2008, 11:56 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •