Results 1 to 5 of 5

Thread: 4 Dof Hexapod Torque calculations

  1. 4 Dof Hexapod Torque calculations

    Hello all,

    I am currently off from college and I am trying to calculate the torque acting on a 4 DOF hexapod has anyone already done this or can help as I'm running in circles with it.

  2. #2

    Re: 4 Dof Hexapod Torque calculations

    Each joint can be individually calculated as if all the other joints are stiff, so I get pretty close by measuring the distance to the base points and the center of mass / weight of the body between the joint and that base point.

    For example, a joint that's right above a foot, actually should get no torque, just down-force, as long as the other joints are rigid.

    This isn't 100% accurate, though -- you really need a CAD package with 3D force/torque analysis to do that.

  3. Re: 4 Dof Hexapod Torque calculations

    Thanks, yeah I think I am doing it right just not had the time to get it done on paper.

    I'm using Solidworks to do my modelling can this be used to torque cals but unsure how to go about so need to play about, what software do you use?

  4. #4

    Re: 4 Dof Hexapod Torque calculations

    Quote Originally Posted by On the Brink View Post
    Thanks, yeah I think I am doing it right just not had the time to get it done on paper.

    I'm using Solidworks to do my modelling can this be used to torque cals but unsure how to go about so need to play about, what software do you use?
    I use a torque calculator by Transducer Techniques. it works great for all my needs

  5. #5

    Re: 4 Dof Hexapod Torque calculations

    The link posted the first time, but all I see is a unit converter, nothing that analyzes the weight distribution of a supported legged robot.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Using AX-12A in zero torque mode.
    By ZanQdo in forum DYNAMIXEL & Robot Actuators
    Replies: 9
    Last Post: 06-20-2015, 03:23 AM
  2. Matrix calculations
    By navidahmeduom in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 05-15-2015, 03:41 PM
  3. Question(s) Quadruped torque calculations - Confirmation Please!!!
    By Ferret in forum Humanoids, Walkers & Crawlers
    Replies: 25
    Last Post: 07-06-2013, 02:41 AM
  4. Servo torque required for hexapod
    By Fatfrank69 in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 02-19-2013, 05:08 PM
  5. Voltage Sensor calculations
    By super-d in forum Sensors
    Replies: 3
    Last Post: 03-01-2008, 11:56 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •