Page 3 of 3 FirstFirst 123
Results 21 to 26 of 26

Thread: mjbots quad A0

  1. #21

    Re: mjbots quad A0

    Looking forward to it!

    You should post it in https://forum.mechwarfare.org/c/builds/6 -- it'll give you a badge ;-)

  2. Re: mjbots quad A0

    More videozzzz:

    Last edited by jpieper; 03-20-2020 at 08:34 AM.

  3. #23
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    858
    Images
    25
    Rep Power
    88

  4. #24
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,312
    Images
    27
    Rep Power
    278

    Re: mjbots quad A0

    Any thoughts on combining two of the servos onto a differential similar to this to make the two-axis joints a bit more compact/robust? I'm thinking more or less a U-shaped bracket with a hard-mount on the base of the U and one servo mounted outside each leg-end with a differential sandwiched/supported between them. Only the horn on the output gear of the differential would be supporting a cantilevered load instead both servo bodies supporting serially connected cantilevered loads.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  5. Re: mjbots quad A0

    I actually had a design nearly exactly like that:

    https://jpieper.com/2019/05/22/resul...er-faire-2019/

    I switched away because I couldn't figure out a way to build one that was suitable for 3d printing.

    https://jpieper.com/2019/05/27/full-...on-leg-design/

  6. #26
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,312
    Images
    27
    Rep Power
    278

    Re: mjbots quad A0

    Not quite what I was thinking of...

    Cannot get image upload as attachment to work right now and getting a mysql error trying to access settings to add an image, but it is literally a U-bracket with two servos mounted to it driving the 'wheels' of a four-gear differential (in a car, it would basically be using the wheels to rotate the body up/down off the ground and control the drive shaft direction). Both servos rotating in same direction moves one axis; servos rotating in opposite directions rotates other (orthogonal) axis. The entire differential can be supported by bigger bearings in the U-bracket than the servos require and the output shaft of the differential can extend through a bearing in the opposite gear to add extra support against the cantilevered load.

    mysqli_query(): (HY000/1030): Got error 28 from storage engine in ..../includes/class_core.php on line 1394
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. mjbots piezo target panels
    By jpieper in forum Mech Warfare
    Replies: 9
    Last Post: 03-27-2017, 05:02 PM
  2. 2 DoF Quad gait
    By ArduTank in forum Mech Warfare
    Replies: 4
    Last Post: 08-01-2013, 07:38 AM
  3. Project small quad
    By inkling in forum Project Showcase
    Replies: 7
    Last Post: 12-08-2011, 07:09 PM
  4. Question(s) Quad balance
    By blastdog in forum Humanoids, Walkers & Crawlers
    Replies: 9
    Last Post: 08-10-2011, 05:11 PM
  5. Just For Fun My Quad
    By blastdog in forum Project Showcase
    Replies: 6
    Last Post: 06-25-2011, 08:07 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •