Looking forward to it!
You should post it in https://forum.mechwarfare.org/c/builds/6 -- it'll give you a badge ;-)
Looking forward to it!
You should post it in https://forum.mechwarfare.org/c/builds/6 -- it'll give you a badge ;-)
More videozzzz:
Last edited by jpieper; 03-20-2020 at 08:34 AM.
Any thoughts on combining two of the servos onto a differential similar to this to make the two-axis joints a bit more compact/robust? I'm thinking more or less a U-shaped bracket with a hard-mount on the base of the U and one servo mounted outside each leg-end with a differential sandwiched/supported between them. Only the horn on the output gear of the differential would be supporting a cantilevered load instead both servo bodies supporting serially connected cantilevered loads.
Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
"You have failed me, Brain!"
[git][mech][hack]
gives free advice only on public threads
I actually had a design nearly exactly like that:
https://jpieper.com/2019/05/22/resul...er-faire-2019/
I switched away because I couldn't figure out a way to build one that was suitable for 3d printing.
https://jpieper.com/2019/05/27/full-...on-leg-design/
Not quite what I was thinking of...
Cannot get image upload as attachment to work right now and getting a mysql error trying to access settings to add an image, but it is literally a U-bracket with two servos mounted to it driving the 'wheels' of a four-gear differential (in a car, it would basically be using the wheels to rotate the body up/down off the ground and control the drive shaft direction). Both servos rotating in same direction moves one axis; servos rotating in opposite directions rotates other (orthogonal) axis. The entire differential can be supported by bigger bearings in the U-bracket than the servos require and the output shaft of the differential can extend through a bearing in the opposite gear to add extra support against the cantilevered load.
mysqli_query(): (HY000/1030): Got error 28 from storage engine in ..../includes/class_core.php on line 1394
Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
"You have failed me, Brain!"
[git][mech][hack]
gives free advice only on public threads
There are currently 1 users browsing this thread. (0 members and 1 guests)
Bookmarks