Results 1 to 2 of 2

Thread: Can't connect to Dynamixel MX-106T servo on dynamanager

  1. Can't connect to Dynamixel MX-106T servo on dynamanager

    Hi all,

    I'm trying to set the id of the widow xl arm servos that had just arrived. This worked with two MX-64, two AX-12A and one MX-106T servo. But the second servo MX106T servo isn't responding. However, when I power that servo I can see that the servo blinks red once as usual to indicate that there's power.

    I'm currently using dynamanager v1.3 on windows and my computer is connected to an Arbotix robocontroller via an FTDI cable. I've also made sure that there is only one servo connected to the robocontroller at any one time. Any help to solve this issue would be much appreciated.

    Thank you
    Alex

  2. #2

    Re: Can't connect to Dynamixel MX-106T servo on dynamanager

    Do you have a USB2Dynamixel or perhaps a U2D2?
    Then you might be able to use the Dynamixel Wizard to see if you can scan to find the servo.
    You can also attempt to update the firmware of the servo.
    If that still doesn't work, then you may have to send the servo to Robotis for warranty service, but it's quite likely that the problem can be fixed with dynamixel manager. It's probably a serial port speed difference, or something like that.
    If you don't have the U2D2, I'd recommend getting it, even though it's $50; it significantly improves the debugging experience when using the dynamixel manager.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Dynamanager finds mx-28t but not mx-106T
    By Trevor in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 1 Week Ago, 07:49 AM
  2. For sale: MX-106T, MX-64T, MX-28T Dynamixel
    By DresnerRobotics in forum Garage Sale
    Replies: 0
    Last Post: 07-07-2017, 08:59 PM
  3. Question(s) MX-106T ID changes issue - the servo not communicate
    By Ecku01 in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 01-25-2017, 04:17 AM
  4. Dynamixel MX-106T with arduino feedback problems
    By mtete in forum Software and Programming
    Replies: 4
    Last Post: 04-27-2016, 12:13 PM
  5. 18 Dynamixel Ax-12A with ArbotiX/Arduino - How to connect the dynamixel?
    By Snuuq in forum Arbotix, Microcontrollers, Arduino
    Replies: 20
    Last Post: 02-14-2014, 11:29 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •