Page 1 of 2 12 LastLast
Results 1 to 10 of 11

Thread: How to make a sensing-sphere???

  1. #1
    projectgrl Guest

    Red face How to make a sensing-sphere???

    Hi all,

    I am new to the forum, and new to robotics, but I thought I may be able to get some advice here...?

    I am a university student completing my thesis in electronic devices for occupational therapy. I am designing a squeezable ball, like a stress-ball, that plays sounds when it is squeezed.

    I would like to apply pressure sensors to the surface of the ball (under a silicone cover or similar) so that different squeezing pressures on different areas of the surface would produce a variety of audible sound outputs.

    The sensors I am considering are 24 Inch Strip FSR Kit (Item: S-20-1000-FSRKT24) or FlexiForce 0-25 lbs. and Resistive Force Sensor (Item #: S-20-1000-FS25LB), however I don't know if they would be suitable... They would have to be wrapped around the ball, and I am concerned that they would not operate underthe non-uniform distortion created by the squeezing forces of the hand.

    Does anyone know if these sensors can be applied in this manner? Either moulded into the plastic (polyurethane) surface, or adhered to an internal frame.

    Or does anyone know of any other technology that may be suitable? e.g. flexible films / 'artificial skin' pressure sensors etc I am having a hard time finding anything that is not still only theoretical in these fields...

    Any advice / information / leads are most appreciated!

    Cheers.

  2. #2

    Re: How to make a sensing-sphere???

    What about a solid core with the sensors mounted on that and then and overcovering of some type of compressible material?

    This way the sensors have a firrm backing so the will not deform when the ball is
    being squeezed.

  3. #3
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    176

    Re: How to make a sensing-sphere???

    Another thing to note: The sensors are not sensitive on their "tails". You'd probably have to consider putting the tails inside the ball.

    How about piezo strain gauges?

    Anyway - you can read about the fsr's here: http://en.wikipedia.org/wiki/Strain_gauge
    I Void Warranties´┐Ż

  4. #4

    Re: How to make a sensing-sphere???

    Based on the Flexi Force Sensors Trossen Sells here (s-20 1000 FS25LB) Which are .55 sq.

    Flexi Force also says you can trim the leads to length.

    The example here is a 3" ball.

    You will have to get some type of rubber or slicone and cast the ball around the sensors.

    How many sensors and the wiring and type of covering will take some experimenting

  5. #5
    Join Date
    Jul 2008
    Location
    Belgium
    Posts
    633
    Images
    2
    Rep Power
    61

    Re: How to make a sensing-sphere???

    If you're only interested in the amount of pressure, and not the direction of the pressure, why not use a hollow silicone ball with an absolute pressure sensor?
    The harder the ball is squeezed, the higher the internal pressure.

    Drawbacks: only a single pressure measurement is taken, direction of the pressure does not play any role, and getting a hollow ball with the internal electronics while at once having a good seal isn't trivial.

    Either way I don't think it's the simplest project to handle hardware-wise, given the amount of abuse a stress-ball usually gets
    Artificial Intelligence is no match for Natural Stupidity

    "For a list of all the ways technology has failed to improve life, press three" - Alice Kahn

    Resistance is futile! (if < 1)

  6. #6
    Join Date
    Nov 2007
    Location
    Sunnyvale
    Posts
    65
    Rep Power
    45

    Re: How to make a sensing-sphere???

    If you're planning to build a lot of them, one cheap approach would be an array of capacitive touch "sensors". A cap touch sensor is just a metal strip -- in fact, you can implement the sensors as metal pads on the PCB inside the ball. With multiple PCB pads/sensors you can detect the position and proximity of fingers even through material 2 inches thick. The Pleo dinosaur uses this approach to sense very light touches above his rubber skin.

    Some microcontrollers have on-chip peripherals for capacitive touch applications. (Cypress PSoC/CapSense, Microchip CTMU.) Also, TI has a great appnote demonstrating how this can be done on a microcontoller with no special peripherals: http://focus.ti.com/lit/ml/slap105a/slap105a.pdf

    - Nathan

  7. #7
    Join Date
    Jun 2008
    Location
    Crabfu's Garage.. <_<
    Posts
    302
    Images
    12
    Rep Power
    45

    Re: How to make a sensing-sphere???

    You could also just do a series of micro switches. That would probably be the simplest approach, at least with me knowing nothing at all about what everyone else is talking about..
    This ain't nothing but a summer jam
    Brown skin and cinnamon tans, whoa!
    This ain't nothing but a summer jam
    We're gonna party as much as we can
    Hey-yeah, ooh, hey-yeah
    Summer jam alright
    Hey-yeah, ooh, hey-yeah

  8. #8
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    176

    Re: How to make a sensing-sphere???

    Microswitches aren't of any value for pressure sensing.
    I Void Warranties´┐Ż

  9. #9
    Join Date
    Jun 2008
    Location
    Crabfu's Garage.. <_<
    Posts
    302
    Images
    12
    Rep Power
    45

    Re: How to make a sensing-sphere???

    Quote Originally Posted by Adrenalynn View Post
    Microswitches aren't of any value for pressure sensing.
    Good point, I missread what she was saying. I thought she wanted different parts to emit different tones..
    This ain't nothing but a summer jam
    Brown skin and cinnamon tans, whoa!
    This ain't nothing but a summer jam
    We're gonna party as much as we can
    Hey-yeah, ooh, hey-yeah
    Summer jam alright
    Hey-yeah, ooh, hey-yeah

  10. #10
    Join Date
    Jul 2008
    Location
    Chicago
    Posts
    307
    Rep Power
    47

    Re: How to make a sensing-sphere???

    The fsr might work but as you mold them in to the rubber type material for the ball you readings would already be off. The pressure of the rubber itself on the sensor. I think the readings wouldnt be accurate but this is something you would need to experiment with. And im sure you could compensate with software as well

    You would need a combination of sensors. I like the pressure sensor in side a tennis ball for example. Motorola makes a barimetric pressure sensor. As long as you have it airtight it would work. You can cut a small slit in it tuck inside hot glue the slit then dip the awhole ball in a rubber dip. Mcmaster sells something like this pretty cheap to 20 for a gallon. Couple of coats and its flexible.

    Then on the outside you would use tactile switches. You could make a matrix around the ball. Then you could even design some software to do a 3d view of the ball and where its being tounched and somehow incoporate the pressure in to color type pattern red for the most blue for the least etc. The you would mold it in the plastic again. the switchs wouldnt be affected as long as you coat the with something so the plastic wont stick to them. Wax or something.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Making Things Controller
    By LinuxGuy in forum Arbotix, Microcontrollers, Arduino
    Replies: 29
    Last Post: 08-06-2008, 05:47 PM
  2. News/Announcement Make TV has callout for projects
    By Matt in forum Robotics General Discussion
    Replies: 2
    Last Post: 08-05-2008, 11:05 PM
  3. SSC-32 issues...it works with the lynxmotion terminal but not with anything I make :-(
    By Superlaxstar112 in forum Arbotix, Microcontrollers, Arduino
    Replies: 6
    Last Post: 07-20-2008, 03:05 AM
  4. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 06:49 PM
  5. Contest Entry Make a wall avoiding robot! Part 1
    By Brandon121233 in forum Project Showcase
    Replies: 16
    Last Post: 09-12-2007, 05:41 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •