Hello,

I set up the IDs of my servos with Dynamixel Wizard 2 one-by-one with U2D2 USB communication converter.

I built my PhantomX-Reactor and connected all servos. My power jumper towards in on 'VIN'. I have the 12V 5A adaptor.
I scanned again the servos with Dynamixel and U2D2. The scan works. I can see my AX-12A servos.

Click image for larger version. 

Name:	dynamixel.jpg 
Views:	82 
Size:	83.1 KB 
ID:	7646

I uploaded the ArbotixBlink sketch from Arduino 1.8.10 to my Arbotix-M card. That works.


I uploaded AXSimpleTest sketch -> "Done compiling" -> "Done uploading". Nothing moves.
I uploaded dxlServoScan. Compiling and uploading works but I have the message in the serial monitor :
Servo ID : Error Bit
1:No Servo Found
2:No Servo Found
3:No Servo Found

I tried a lot of sketchs and my servo ID 1 is never found. What do I have to check ? I really need help please.