Hi,

I'm working on a project using an Arbotix Pro connected to multiple MX106T motors. I tried to update the firmware for the motors using Dynamixel Wizard 2.0, my Arbotix Pro was connected to my PC via micro USB. But the update failed and now I can't see my servos in Dynamixel Wizard 2.0 and even 1.0, even if Dynamixel power is set to 1 in my Arbotix Pro. I tested the motors by connecting another controller and I could see them in Dynamixel Wizard. So is my Arbotix Pro firmware broken? The board seems fine and is recognized but the servomotors connected aren't recognized anymore. What would be a solution to this problem ?