Results 1 to 4 of 4

Thread: How useful are broadcast ID, Bulk Read/Write and Sync Read/Write? How often do people use them?

Hybrid View

Previous Post Previous Post   Next Post Next Post
  1. How useful are broadcast ID, Bulk Read/Write and Sync Read/Write? How often do people use them?

    Hi, how often do all of you use these commands? Are these commands useful in controlling a robot with many motors? By using these commands, can I ask different motors to move differently at the same time? When and how often are these commands being used?

  2. #2
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    858
    Images
    25
    Rep Power
    88

    Re: How useful are broadcast ID, Bulk Read/Write and Sync Read/Write? How often do people use them?

    I use them all the time. It's the most efficient way to communicate. Especially when you are using it for a walking robot.

  3. Re: How useful are broadcast ID, Bulk Read/Write and Sync Read/Write? How often do people use them?

    Thanks KevinO.

  4. #4

    Re: How useful are broadcast ID, Bulk Read/Write and Sync Read/Write? How often do people use them?

    I use broadcast ID a lot, and sync write for writing a pose quicker than writing each servo individually. I don't use protocol 2.0, so I don't use bulk read.

    Broadcast ID is cool for things like "blink the LEDs of all servos" and "enable or disable torque for all servos at the same time."
    Given that I see up to 2% packet loss under movement at times, I will frequently send the broadcast packets on a repeating schedule, saying "set the state to X," rather than assuming that the first packet always makes it. Separately, for sync write, because animation updates the bus quickly (50-100 times a second,) that kind of takes care of itself.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Dynamixel bulk read behavior on missing servo
    By daviherc in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 06-06-2018, 07:32 AM
  2. Replies: 1
    Last Post: 08-15-2014, 07:03 PM
  3. AX12A sync write
    By DVS in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 08-14-2013, 09:15 PM
  4. Interesting Write LMR challenge
    By Xan in forum Robotics General Discussion
    Replies: 6
    Last Post: 09-16-2008, 11:10 AM
  5. Question(s) Cannot figure out how to write to the serial port in C++
    By Superlaxstar112 in forum Software and Programming
    Replies: 4
    Last Post: 07-23-2008, 05:02 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •