Results 1 to 4 of 4

Thread: Robot Body Shell

  1. Robot Body Shell

    I am interested in building a custom exterior body shell for my robot. I was wondering if anyone has had any luck with poured resin or plastic molds. I have seen a few things on the internet, however it seems you have to get into alot of hardware before you can even start. I started making a white styrofoam shell that is easy to form however it would not hold up with prolonged use, I was going to put a skim coat of auto body putty over it that would give me a finished and paintable shell. But this would increase the weight of the robot and I want to keep it light. Any suggestions would be great.

    LLRB

  2. #2
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    95

    Re: Robot Body Shell

    I 3D printed mine. But I did consider making it a negative and making it a mold for a moment.

  3. #3
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    95

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    284

    Re: Robot Body Shell

    I'm a fan of the rutan 'cast/carve foam into shape then coat with fiberglass+resin' construction method, but not used it for robots yet. The resulting composite is very stiff and lightweight (good enough for 'unsinkable' boats and custom airplanes and cars), but can be a bit messy if using styrofoam blocks requiring much material removal.

    Polycaprolactone (PCL, instamorph, etc.) is another material useful for building durable, flexible shells although its biodegradable property means it can easily become coated in biomass when stored in wet conditions. It also has vicious bonding/adhesion to most other plastics when molten so have to be careful trying to mold it around something else if you do not actually want it bonding to that object. It works especially well if looking for cheap/organic designs without access to a 3D printer and can be used to make molds for casting other materials if properly coated with release agents.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Z-363 Spectre 3D Printed Body for Bioloid Premium
    By CasperH in forum Project Showcase
    Replies: 18
    Last Post: 07-09-2016, 12:14 PM
  2. Robotis CM-700 Shell ?
    By Ron in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 11-15-2012, 06:28 PM
  3. GM10 robot body
    By Rbotguy in forum Garage Sale
    Replies: 0
    Last Post: 01-20-2011, 09:54 PM
  4. Towards a body-worn wireless arm controller
    By Adrenalynn in forum Project Showcase
    Replies: 59
    Last Post: 01-16-2009, 09:32 PM
  5. Robot Body Shell
    By Tymtravler in forum Robotics General Discussion
    Replies: 3
    Last Post: 11-26-2007, 04:51 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •