Results 1 to 7 of 7

Thread: Is it easy to change the adapter of those Robotis cables?

  1. Is it easy to change the adapter of those Robotis cables?

    Hi, I need convertible cables longer than the 180mm one sold by Robotis. is it easy to remove the connectors from Robotis current cables for the X-series and older cables with MOLEX connectors? Any recommended tools?

  2. #2

    Re: Is it easy to change the adapter of those Robotis cables?

    If you need custom cables, you'll want to buy the crimping kits for the connector series from the manufacturer, and your own wire to crimp the cables onto.
    The main challenge there is generally the actual crimp tool, where the manufacturer sometimes charges thousands of dollars for what's essentially a pair of pliers with a die on them. There are often third-party options that are much more reasonable.

    What I do when I just need one or two extra-long cables, is to get two cables, cut each next to the unwanted connector, and then splice them with some solder and shrinkwrap. E g, two cables that are 180 mm of "A -- B" would turn into "A --" and "-- B" and then be spliced into a 340mm cable "A -- -- B". (There's always some length loss.)

  3. Re: Is it easy to change the adapter of those Robotis cables?

    Quote Originally Posted by jwatte View Post
    If you need custom cables, you'll want to buy the crimping kits for the connector series from the manufacturer, and your own wire to crimp the cables onto.
    The main challenge there is generally the actual crimp tool, where the manufacturer sometimes charges thousands of dollars for what's essentially a pair of pliers with a die on them. There are often third-party options that are much more reasonable.

    What I do when I just need one or two extra-long cables, is to get two cables, cut each next to the unwanted connector, and then splice them with some solder and shrinkwrap. E g, two cables that are 180 mm of "A -- B" would turn into "A --" and "-- B" and then be spliced into a 340mm cable "A -- -- B". (There's always some length loss.)
    Thanks. I made custom cables many years ago. I know that I am not very good at it.

    Is it a bad idea to change the connectors soldered in the hub or controller board instead?

    What is the name of those net-like sleeve that can be used to cover those thinner robotis cables?
    Last edited by Snoopy; 06-03-2020 at 02:54 PM.

  4. #4

    Re: Is it easy to change the adapter of those Robotis cables?

    Net-like sleeves are called "cable sleeving" or "cable sheathing."
    https://www.mcmaster.com/cable-sheathing/
    https://amzn.to/30f5w8y

  5. Re: Is it easy to change the adapter of those Robotis cables?

    Thank you

  6. Re: Is it easy to change the adapter of those Robotis cables?

    Hi jwatte, McMaster sells so many different types of cable sheathings. Which one do you recommend?

  7. #7

    Re: Is it easy to change the adapter of those Robotis cables?

    Bob's Used Cars sell so many kinds of used cars and trucks, which one would you recommend?

    I recommend that you buy the one that seems to work for your application.

    If you have a hard time making up your mind, pick three or four and buy a small amount of each, to get your hands on them and check out which one will work best for you.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Current rating of dynamixel cables
    By Janis in forum Power
    Replies: 3
    Last Post: 03-03-2013, 08:38 PM
  2. AX-12 Cables
    By sarendt in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 03-15-2011, 04:14 AM
  3. Trouble with AX-12+ cables & connectors
    By Pi Robot in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 07-10-2010, 08:55 PM
  4. Question(s) RX-64 4-pin connector cables
    By dsahm in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 07-24-2009, 01:26 PM
  5. Question(s) Extending servo cables
    By Dementedwombat in forum Robotics General Discussion
    Replies: 8
    Last Post: 01-24-2009, 09:09 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •