Results 1 to 8 of 8

Thread: How to test Dynamixels upon arrival

  1. How to test Dynamixels upon arrival

    Hi, when receiving expensive Dynamixels, what should one check to make sure that they arrived without any issue? Is updating the firmware the first thing to do?

  2. #2

    Re: How to test Dynamixels upon arrival

    I sometimes just run one of my own test sketches, that does something like: scan at the default baud rate to find any servo. It should find it probably as ID #1.

    I then have my test program, maybe do set the ID, set my desired baud rate, and depending on servos set the respond time... Then try a couple of moves to make sure that it works that way...

    Other times I use the Robotis sketches to do the same or their PC program.

    Again nothing special. So far I have only had one DOA servo sort of (I think it worked for a couple of tests and then died...
    MX12W...

  3. Re: How to test Dynamixels upon arrival

    Thanks KurtEck.

  4. Re: How to test Dynamixels upon arrival

    Is it recommended to always update the firmware upon receiving the dynamixels?

  5. #5

    Re: How to test Dynamixels upon arrival

    I did not always do it... Only if there looks like they have new features or important bug fixes. But with some of their newer servos I tended to update them when I could.

    But sometimes I go by the: If it ain't broke don't fix it...

  6. Re: How to test Dynamixels upon arrival

    Thanks

  7. #7
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    95

    Re: How to test Dynamixels upon arrival

    If it is MX and you want to use Protocol 2.0 you might have to update it. Plus Protocol 2.0 is miles better than 1.0. It's fantastic so many new features.

  8. Re: How to test Dynamixels upon arrival

    Thanks Kevin.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Bad luck with Dynamixels?
    By tigakub in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 05-30-2015, 07:35 PM
  2. Is there an HR-OS5 electronics kit for those who already own Dynamixels?
    By robot_yan in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 12-24-2014, 08:37 AM
  3. Question(s) TTL communication in Dynamixels?
    By Robotronn in forum Robotics General Discussion
    Replies: 1
    Last Post: 11-25-2014, 11:17 PM
  4. Question(s) Battery recommendation for mx-64t dynamixels
    By adityassripada in forum Power
    Replies: 1
    Last Post: 07-03-2014, 07:21 PM
  5. Micro-size Dynamixels ?
    By kert in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 10-04-2011, 06:00 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •