Results 1 to 7 of 7

Thread: Linux install

  1. #1
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    52

    Linux install

    So I was planning on getting a gumstix verdex as soon as my next paycheck comes in, but I realized that I don't know to much about linux. From what I have read so far I need to have linux on a host computer so that I can setup the gumstix. Here in lies the problem. My computer has windows xp on it right now and I am not about to just get rid of it. I downloaded Ubuntu 8. Could someone explain for me how to steup my computer so I can dual-boot?

  2. #2

    Re: Linux install

    When you install Ubuntu, there should be an option to set up your computer to dual boot. Don't be afraid to install linux. Just set aside a partition for it to go on your hard drive, choose that particular partition when you install linux and you shouldn't have a problem. When you start the computer it should come up with the boot loader screen and you can choose whichever OS you want (linux will be the default unless you manually change that). All the dual boot setup will be handled by the linux installation.

  3. #3
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    127

    Re: Linux install

    There are a few steps in the install:

    First - AND MOST IMPORTANT - back everything up! Make sure you have backups of every file you ever created, make sure you have install disks or files for anything you want to put back on - remember, windows apps typically have lots of pesky configuration files you may want to save...

    Second - check that you backed everything up! I'm serious, if something goes wrong during repartitioning or installing the boot loader you are screwed...

    Third - Defrag the windows partition, so that everything moves to the front of the drive...

    Fourth - Repartition. We need a dedicated space for Linux. Depending on the distribution of Linux you choose, many have this repartition package built into the installer

    Fifth - Install - with most modern *nix distros the installer is very good and straight-forward (no worse than installing a Windows OS). This installer will make typically have 10-15 steps within it, to decide where to put stuff and how much stuff to put there...

    For a first time Linux user, I would recommend using Ubuntu, or another easy to install Linux Distro. You may also want to check your hardware to see that it is supported under linux. In particular, things like high-end video and sound may have limited support (and may thus not function at their best). One last consideration - make sure you have another computer available to get online to look stuff up - just in case something goes awry...

    -Fergs

  4. Re: Linux install

    I do not know if it will work but on option is maybe to use a virtual machine that’s running Linux.
    One open source software that enable you to create and run linux as a guest operating system is VirutalBox http://www.virtualbox.org/

    /Marcus

  5. #5
    Join Date
    Jan 2007
    Location
    Near Robot Parts In The USA
    Posts
    232
    Rep Power
    46

    Re: Linux install

    There is a very easy way which is included on the Ubuntu 8.04 install disk:

    Download the ISO, burn the ISO (don't copy), insert the newly burned disk, a window should pop up asking what you want to do, select the install as program option (or something like that), now you can boot into Linux or XP! If you ever want to uninstall you can do that within Windows.

    No splitting drives, copying over Windows, etc!
    Dell Studio XPS Desktop, Windows Vista, 12 GB RAM, 2x 500 GB SATA RAID0 HDD, Intel i7 2.66Ghz Quad Core (4 cores, 8 virtual cores). The power that's needed... plus some!

    RIBO Labs, Springing Robotic Development to a New Level

  6. #6
    Join Date
    Sep 2008
    Location
    The devil steals my soul when I go to San Bernardino
    Posts
    109
    Images
    2
    Rep Power
    43

    Re: Linux install

    Ubuntu is a "live cd", you may not need to actually _install_ it anywhere (unless you want to). Boot up with the CD in the drive and poke around and see what you think. This will let you know how well supported your hardware is before getting too deep. While it will run more slowly from the CD than from hdd, it's still a useable option for those not wanting to leave Windows. You may be able to run the gumstix software that way, but it won't be a persistent "install", you'd have to re-install gumstix every time you wanted to play.

    If you like it and want to install, I'll second lnxfergy's third step, make sure to defrag your windows install first! Then when you run Ubuntu's installer it will give you the option of (non-destructively) repartitioning your windows partition and installing Ubuntu to the new free space. It'll also import your Windows preferences, bookmarks, etc... if you want.
    Earth's got chinese food and microphones.
    Earth's got porno stars and ice cream cones...

  7. #7
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    127

    Re: Linux install

    Yeah, the Live CD will let you poke around in Ubuntu and try it out, but I would say you want to install it to do gumstix work...

    On that note, Linux doesn't require much computing power - got an older computer just sitting around looking to be used?

    -Fergs

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) whats a good linux system for robots
    By robot maker in forum Software and Programming
    Replies: 3
    Last Post: 08-30-2008, 10:16 PM
  2. Discussion Linux Robots
    By LinuxGuy in forum Robotics General Discussion
    Replies: 15
    Last Post: 04-02-2008, 09:32 AM
  3. Question(s) Linux and Phidgets
    By LinuxGuy in forum Sensors
    Replies: 1
    Last Post: 03-24-2008, 11:08 AM
  4. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •