Results 1 to 5 of 5

Thread: Tachikoma by TheMaverick

  1. #1
    Join Date
    Aug 2020
    Location
    Stuttgart, Germany
    Posts
    3
    Rep Power
    0

    Tachikoma by TheMaverick

    Hi Everyone,
    this is my first post here. I Want to show you my current Tachikoma Projekt.
    Since March 2020 i am designing the Body parts for a large Tachikoma.
    From front left Leg to rear right Leg it will have a diameter of around 80cm.

    Each Leg got 4 servos. Two of them you can see, the other two are inside of the balljoints.
    I scaled the Tachikoma model up till classic 9g Servo fit into the balljoints. every thing else came afterwards.



    While constructing and test-print of some prototypes i created a iOS Application to test the Actuator Ranges. I Have done some Videos of it.



    Hope you like this Project.
    This is my first Project i ever did with fusion 360 and my fist 3d construction since 2005 (3D Studio Max).

    I am a professional iOS Mobile Developer so i will use a lot of the computing power of my phone and less of the power of the esp32 inside the Tachikoma. The "simulator" of the phone will be also the remote control for the real live version of it.

  2. #2
    Join Date
    Aug 2020
    Location
    Stuttgart, Germany
    Posts
    3
    Rep Power
    0

    Re: Tachikoma by TheMaverick

    Click image for larger version. 

Name:	IMG_7013.jpg 
Views:	533 
Size:	125.8 KB 
ID:	7663First Prototype prints of my fake-balljoint. inside the center piece i added a 9g servo. because i did not know how to fix the servo on the outer shell, i used a placeholder for a generic servo head. on the other side i added a ball bearing to remove weight from the servo.

  3. #3
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    124
    Images
    1
    Rep Power
    19

    Re: Tachikoma by TheMaverick

    That's pretty neat! And cool to see you playing to your strengths (iOS)

  4. #4

    Re: Tachikoma by TheMaverick

    That sounds fantastic!

    classic 9g Servo fit into the balljoints
    Have you done the torque calculations? Will 9g servos be able to hold this design without overheating?

  5. #5
    Join Date
    Aug 2020
    Location
    Stuttgart, Germany
    Posts
    3
    Rep Power
    0

    Re: Tachikoma by TheMaverick

    No i did not. Not my profession. I use metal gear 9g with a torque of 3kg/cm. I hope this is enough.
    Try and Error till it burns

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Tachikoma
    By CasperH in forum Humanoids, Walkers & Crawlers
    Replies: 105
    Last Post: 05-05-2016, 06:01 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •