Results 1 to 2 of 2

Thread: Connect servo dynamicel XL-320 to wizard 2.0 without U2D2

  1. Question Connect servo dynamicel XL-320 to wizard 2.0 without U2D2

    Hello all,

    I would like to control my XL-320 (https://emanual.robotis.com/docs/en/dxl/x/xl320/) with the Wizard 2.0 (https://emanual.robotis.com/docs/en/.../#introduction) without U2D2 nor USB2Dynamixel.

    Has anyone ever done this ?

    I tried with an SN74LS241N chip and failed.

  2. #2

    Re: Connect servo dynamicel XL-320 to wizard 2.0 without U2D2

    What is the actual challenge here? You can't just use a 74241, you need a USB UART adapter, which shows up as a COM port in Windows. Then you point the Robotis software at that COM port. Then you need that UART to know whether it's sending or receiving bytes -- a typical FTDI or CPI2101 serial port adapter won't do this, so you'll likely want to use an Arduino Leonardo or PJRC Teensy microcontroller, so you can set the "transmit direction" appropriately based on whether there's data to put on the wire, or you've sent the final stop bit.

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. Question(s) Can't connect to Dynamixel MX-106T servo on dynamanager
    By ADR in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 10-02-2019, 04:03 PM
  2. Question(s) U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012
    By jcarlos in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 07-13-2019, 03:57 PM
  3. Question(s) Can't connect the servo after input voltage error
    By Liang Shan in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 05-07-2019, 03:01 PM
  4. RX-28 Roboplus Manager works but Wizard and SDK have problem
    By HSB in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 02-17-2016, 03:38 PM
  5. Question(s) Not Able to Find AX-12A servo with Dynamixel Wizard
    By chenji28 in forum DYNAMIXEL & Robot Actuators
    Replies: 14
    Last Post: 12-31-2015, 12:31 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •