Results 1 to 4 of 4

Thread: Serial Monitor keeps printing reversed question marks when using the DynamixelShield with UNO

  1. Serial Monitor keeps printing reversed question marks when using the DynamixelShield with UNO

    please remove
    Last edited by Snoopy; 09-20-2020 at 05:04 PM.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: Serial Monitor keeps printing reversed question marks when using the DynamixelShield with UNO

    How is it so damn difficult for you to read instructions? Over and over and over on multiple topic and multiple forums...

    quoth the e-manual (https://emanual.robotis.com/docs/en/...ixel_shield/):
    The hardware serial port is used to communicate with DYNAMIXEL, therefore, RC-100 or LN-101 has to be connected to the software serial communication port(SW TX/RX) via Arduino pin 7 and 8.
    There is only one hardware serial port on the UNO. It is connected to a USB to UART IC to give a virtual serial port used for programming and Arduino IDE Serial Monitor. It is also always being used for controlling the dynamixel buss, so cannot be connected to the Serial Monitor for debug output. You need an LN-101 or similar USB to UART adapter to connect to the software serial port to get the debug output (and cannot be used for programming the Arduino UNO).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: Serial Monitor keeps printing reversed question marks when using the DynamixelShield with UNO

    Also, don't remove a question just because it's answered. Others on the internet have the same question. If it's not preserved in the thread, google won't find it the next time around, and the cycle repeats.

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: Serial Monitor keeps printing reversed question marks when using the DynamixelShield with UNO

    ...or have to ask questions multiple times over pm because older messages were lost or deleted.


    DATA PACK RAT FOREVER!
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. When do we use a LIPO monitor?
    By Snoopy in forum Power
    Replies: 4
    Last Post: 02-16-2016, 05:16 PM
  2. Device to monitor battery
    By Snoopy in forum Power
    Replies: 3
    Last Post: 08-17-2015, 10:35 PM
  3. Question about multidrop TTL serial (dynamixel UART)
    By erazor in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 08-24-2013, 04:37 PM
  4. Question(s) Arduino IDE Serial Monitor output on Linux
    By Stephen in forum Software and Programming
    Replies: 5
    Last Post: 10-02-2010, 05:55 PM
  5. Replies: 7
    Last Post: 07-31-2008, 01:03 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •