please remove
please remove
Last edited by Snoopy; 09-20-2020 at 04:04 PM.
How is it so damn difficult for you to read instructions? Over and over and over on multiple topic and multiple forums...
quoth the e-manual (https://emanual.robotis.com/docs/en/...ixel_shield/):
There is only one hardware serial port on the UNO. It is connected to a USB to UART IC to give a virtual serial port used for programming and Arduino IDE Serial Monitor. It is also always being used for controlling the dynamixel buss, so cannot be connected to the Serial Monitor for debug output. You need an LN-101 or similar USB to UART adapter to connect to the software serial port to get the debug output (and cannot be used for programming the Arduino UNO).
Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
"You have failed me, Brain!"
[git][mech][hack]
gives free advice only on public threads
Also, don't remove a question just because it's answered. Others on the internet have the same question. If it's not preserved in the thread, google won't find it the next time around, and the cycle repeats.
...or have to ask questions multiple times over pm because older messages were lost or deleted.
DATA PACK RAT FOREVER!
Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
"You have failed me, Brain!"
[git][mech][hack]
gives free advice only on public threads
There are currently 1 users browsing this thread. (0 members and 1 guests)
Bookmarks