Results 1 to 2 of 2

Thread: Help! PhantomX with PS2 Controller

  1. Help! PhantomX with PS2 Controller

    Hello,

    I am trying to use a lynxmotion ps2 controller with the Arbotix-m Hexapod. I have been able to get a connection but the data ia not being recieved. I am using the ps2 test code. The one thing I notice is that the PS2 is used with the botboarduino which has a built in pull-up resistor for the DAT pin. Can I shimmy a 1K resistor in with the PS2? I would have to splice the 5v wire? Since Trossen no longer has the controller, I need to find a good wireless way to control the bot. Any help would be appreciated.

    I have thought of using an XBee with the GoBLE app that is similar to a arbotix commander/ps2.

  2. #2

    Re: Help! PhantomX with PS2 Controller

    I just finished putting together the Mark III Hexapod and got it working and writing C code for it. This is the next thing I sorely want to do - a PS2 (or above) controller, so I'm also searching. I'll keep an eye on this and if I find anything I'll post it.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX + CM9.04 but no Xbee!
    By ptegler in forum Humanoids, Walkers & Crawlers
    Replies: 9
    Last Post: 12-11-2018, 06:28 PM
  2. Question(s) PhantomX AX Quadruped Mark II PhantomX Robot Turret Equipped??
    By hwan we in forum Robotics General Discussion
    Replies: 1
    Last Post: 03-11-2013, 03:09 PM
  3. For learning: PhantomX Hexapod vs PhantomX Quadruped
    By Leugim in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-26-2012, 09:50 AM
  4. Question(s) PhantomX with TurtleBot Arm
    By dyrge in forum Robotics General Discussion
    Replies: 3
    Last Post: 09-03-2012, 10:34 PM
  5. Question(s) Motor Controller. Do I need a servo controller too?
    By kankatee in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 11-14-2008, 11:03 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •