Currently struggling to connect the VX300s 6DOF robot. The operating system running is Ubuntu 18.04. This install script from the ros manipulators repository was successfully executed on the machine. Observing the udev rules shows the interbotix rules were copied correctly. However I can never see /dev/ttyDXL when the robot is connected. Running lsusb does show the device is connected to the motherboard properly.
Code:
Bus 007 Device 002: ID 0403:6014 Future Technology Devices International, Ltd FT232H Single HS USB-UART/FIFO IC
Power is supplied and a red light appears on the U2D2.


Below is the error that I receive when trying to launch the moveit interface. Any suggestions to resolve this would be wonderful. Thanks!

Bookmarks