Results 1 to 2 of 2

Thread: PhantomX Reactor -> USB2AX -> Arm Link ->Processing 3 -> Windows 10 (is this possible?)

  1. PhantomX Reactor -> USB2AX -> Arm Link ->Processing 3 -> Windows 10 (is this possible?)

    A friend gifted me a Reactor Arm with 8 servos.

    I got the USB2AX driver installed under Windows 10 (COM4)

    Using RoboPlus 1 Dynamixel Wizard, I can see the COM4 working since it updates the encoder positions if I move joints by hand.

    I installed Processing3 and the G4P and video libraries.
    Then I downloaded ArmLink (https://github.com/Interbotix/ArmLinkSoftware).
    You have to change all instance of G4P.WARNING in the source code to G4P.WARN_MESSAGE
    and then it will run.

    It fails to talk to robot when you click Connect on COM4.
    I get the same verifyPacket Error: No Header! error as this guy:
    https://github.com/Interbotix/ArmLinkSoftware/issues/1


    looking for insight.....
    cheers
    mlewis

  2. #2

    Re: PhantomX Reactor -> USB2AX -> Arm Link ->Processing 3 -> Windows 10 (is this possible?)

    Sorry, did not see this messages until yesterday. Not sure if it was moderated until then.

    There are very few of us up on this forum these days, and I am not sure I can help much, as I no longer have an arm setup, never tried the Arm Link stuff and have never used processing.

    Unfortunately it looks like the library has not been touched in probably at least 5 years, is in an archived state and the developer of it, I am pretty sure has not worked there in a long time.

    It looks like the code was developed for Processing 2, don't know how much of a difference this makes.

    Sorry I am not a help here.

    kurt

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX Reactor - Servos Not Numbered?
    By wookiefurball in forum Robotics General Discussion
    Replies: 1
    Last Post: 05-20-2019, 10:48 PM
  2. PhantomX Reactor, ROS, MoveIt
    By Adam Glass in forum Interbotix Robotic Arms
    Replies: 8
    Last Post: 09-20-2018, 09:54 PM
  3. Question(s) PhantomX Turret - Coding + serial communication through Arduino IDE and Processing
    By Stuck in forum Robotics General Discussion
    Replies: 1
    Last Post: 11-30-2014, 12:37 AM
  4. Playing with the PhantomX Reactor
    By Xevel in forum Interbotix Robotic Arms
    Replies: 6
    Last Post: 03-16-2013, 07:24 PM
  5. 3D Model of the PhantomX Reactor Arm
    By nckswt in forum Interbotix Robotic Arms
    Replies: 5
    Last Post: 12-31-2012, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •