Results 1 to 2 of 2

Thread: Calculating next position for 3DOF arm

  1. Calculating next position for 3DOF arm

    Hi all, first, I have two versions of my question: 1) what is wrong with the way I am trying to calculate the Jacobian and then its pseudo inverse? 2) Does anyone have a good reference for how to solve for the next angles of each joint based on the velocity of the end effector and Jacobian?

    Now some background: I am working on a hexapod and trying to design the inverse kinematics and path following for the individual legs. Because this will involve a lot of repletion/trial and error, I am designing a simulator to help me test my pathing so I don’t accidentally break something. I’ve laid the groundwork for a lot of it; drawing the robot, homogenous transform calculation, even calculating the Jacobian.

    What I’m running into is trouble solving for the inverse Jacobian. The first time it’s calculated seems fine and the arm moves a little bit toward its target. The second time it’s calculated, the values go to extremes causing the arm to basically invert itself. The third and subsequent times, it seems fine.

    I’ve reviewed formulas, not seeing any issue there. I’ve reviewed outputs and haven’t found anything out of the ordinary besides the pseudo inverse. And the visuals appear to make sense after the inversion of the arm.
    I’ve done a lot of research for examples of inverse Jacobian math but can only find symbolic solutions.
    Is there something I’m missing? Code provided below, I’ll mention this is in Ocatave/Matlab.



    Code:
    clc;
    clear;
    clearvars;
    
    
    function H = Hg(th,a,r,d) % Creates homogenous transform
      H = [cosd(th) -sind(th)*cosd(a) sind(th)*sind(a) r*cosd(th);
          sind(th) cosd(th)*cosd(a) -cosd(th)*sind(a) r*sind(th);
          0 sind(a) cosd(a) d;
          0 0 0 1];
    end
    
    
    function drawLeg(t, xp, yp, zp, Body, CoxaS, FemurS, TibiaS, EndEfS)
      CoxaV = [CoxaS(1), FemurS(1); CoxaS(2), FemurS(2); CoxaS(3), FemurS(3)];
      FemurV = [FemurS(1), TibiaS(1); FemurS(2), TibiaS(2); FemurS(3), TibiaS(3)];
      TibiaV = [TibiaS(1), EndEfS(1); TibiaS(2), EndEfS(2); TibiaS(3), EndEfS(3)];
      
      
      plot3(xp, yp, zp, 'b.') %draw path
      hold on
      plot3(CoxaV(1,:), CoxaV(2,:), CoxaV(3,:), 'm', 'LineWidth', 3) %draw coxa
      plot3(FemurV(1,:), FemurV(2,:), FemurV(3,:), 'g', 'LineWidth', 3) %draw femur
      plot3(TibiaV(1,:), TibiaV(2,:), TibiaV(3,:), 'r', 'LineWidth', 3) %draw tibia
      axis([Body(1)-5 Body(1)+5 Body(2)-5 Body(2)+7 Body(3)-5 Body(3)+5])
      axis equal
      %body centered graph to make sure it stays in view while walking
      grid on
      hold off
      pause(t)
    end
    
    
    function [Th1, Th2, Th3] = stepLeg (t, Th1, Th2, Th3, x, y, z)
      ### DESIGN ROBOT ###
      % 3DOF articulting arm
      % Start with only z offset for center of robot.
      x00 = 0; 
      y00 = 0;
      z00 = .5;
    
    
      % Link lengths
      a0 = 2; %distance from body center to leg 1, UPDATE FROM CAD
      a1 = .5; %length of coxa in cm aka base (joint 0) to joint 1 in z direction
      a2 = 1; %length of femur
      a3 = 1; %length of tibia
    
    
      ## DH Parameters ##
      Th0 = 30; %UPDATE FROM CAD
      A0 = 0;
      A1 = 90;
      A2 = 0;
      A3 = 0;
      r0 = a0;
      r1 = 0;
      r2 = a2;
      r3 = a3;
      d0 = 0;
      d1 = a1;
      d2 = 0;
      d3 = 0;
      
      ## Build vectors for each segment ##
      % Each line has an extra element to help the matrix math
      Body = [x00; y00; z00; 1];
      Coxa = [0; a1; 0; 1];
      Femur = [a2; 0; 0; 1];
      Tibia = [a3; 0; 0; 1];
    
    
      ## Generate all homogenous transforms ##
      Hb0 = Hg(Th0, A0, r0, d0);
      H01 = Hg(Th1, A1, r1, d1);
      H12 = Hg(Th2, A2, r2, d2);
      H23 = Hg(Th3, A3, r3, d3);
      Hb1 = Hb0*H01;
      Hb2 = Hb0*H01*H12;
      Hb3 = Hb0*H01*H12*H23;
    
    
      ## Calculate starting locations for each segment ##
      CoxaS = Hb0*Body;
      FemurS = Hb0*H01*Coxa;
      TibiaS = Hb0*H01*H12*Femur;
      EndEfS = Hb0*H01*H12*H23*Tibia;
    
    
      ## Draw the leg ##
      drawLeg(t, x, y, z, Body, CoxaS, FemurS, TibiaS, EndEfS)
      
      ### Now to give a target for the leg ###
      ## Generate Jacobian ##
      # Rotation matrices #
      Rbb = [1, 0, 0; 0, 1, 0; 0, 0, 1];
      Rb0 = Hb0(1:3, 1:3); %use first three rows and first three columns
      Rb1 = Hb1(1:3, 1:3);
      Rb2 = Hb2(1:3, 1:3);
    
    
      # Displacement vectors #
      dbb = 0;
      db0 = Hb0(1:3, 4); %use first three rows of fourth column
      db1 = Hb1(1:3, 4);
      db2 = Hb2(1:3, 4);
      db3 = Hb3(1:3, 4);
    
    
      # Joint rotation velocity matrices #
      rbb = Rbb*[0;0;1];
      rb0 = Rb0*[0;0;1];
      rb1 = Rb1*[0;0;1];
      rb2 = Rb2*[0;0;1];
    
    
      # Create the culumns representing partial diffferentials for each joint #
      %zeroth = [cross(rbb, db3-dbb); rbb] % not needed since it's a fixed joint
      first = [cross(rb0, db3-db0); rb0];
      second = [cross(rb1, db3-db1); rb1];
      third = [cross(rb2, db3-db2); rb2];
    
    
      # Concatinate into the jacobian #
      fullJ = [first, second, third];
      % only need the cartesian portion
      J = fullJ(1:3, 1:3)
      Jinv = pinv(J) %Print for troubleshooting
      
      ## Calculate the velocity of the end effector ##
      EndEfS %Print for troubleshooting
      TargetX = x(1) %Print for troubleshooting
      TargetY = y(1) %Print for troubleshooting
      TargetZ = z(1) %Print for troubleshooting
      Err =[x(1); y(1); z(1); 0] - EndEfS %Print for troubleshooting
      fullV = ([x(1); y(1); z(1); 0] - EndEfS)*t;% Calculate velocity of EE
      V = fullV(1:3); % Removing the last element since it's trash info
    
    
      # Calc new joint angles #
      w = pinv(J)*V; % Calc joint velocities
      delTh = w.'/t % Calc change in joint angles
      Th0 = Th0; %this should never change?
      Th1 = Th1 + delTh(1);
      Th2 = Th2 + delTh(2);
      Th3 = Th3 + delTh(3);
    end
    
    
    
    
    ### TIME STEP ###
    t = .001
    
    
    ### BUILD PATH ###
    % test to determine how piecewise funcitons would work to create path.
    % This square looks really nice for now
    for i = 1:96
      if i <= 24
        x(i) = i/6;
        y(i) = 3;
        z(i) = 1;
      elseif 24 < i  && i <= 48
        x(i) = x(i-1);
        z(i) = z(i-1)+1/6;
        y(i) = 3;
      elseif 48 < i && i <= 72
        x(i) = x(i-1) - 1/6;
        z(i) = z(i-1);
        y(i) = 3;
      elseif 72 < i && i <= 96
        x(i) = x(i-1);
        z(i) = z(i-1) - 1/6;
        y(i) = 3;
      end
    end
    
    
    ### Set Up Initial Angles ###
    % Starting angles
    Th1 = 60; %UPDATE FROM CAD
    Th2 = 0;
    Th3 = 0;
    
    
    ### Time Loop ###
    for i = 1:10
      [Th1, Th2, Th3] = stepLeg(t, Th1, Th2, Th3, x, y, z)
    end

  2. #2

    Re: Calculating next position for 3DOF arm

    The only way to debug code like this, is to print out the intermediate state of the variables, for each time step, with appropriate mark-up to know what-and-when, and then go over it with a fine-toothed comb. Printing in a format that easily loads into Excel or Google Sheets can help.

    However -- when solving leg IK, I have had much more success solving each joint in its own space as a simple quadratic equation (two-bone IK.) Because the joints are orthogonal to each other, and typically the body joint rotates in the ground plane, and all the following joints rotate in the leg plane, the solution is simply:
    1) Rotate the body joint to point at the target point on the ground plane projected to the body plane. Because the point is projected to the body plane, this is a 2D solution. This also puts all the other joints in the leg plane already!
    2) Rotate the leg joints in the leg plane, to put the end (toe, effector, whatever) at the ground point, in the leg plane -- this is a 2D solution, not a 3D solution!

    Once you think of it like this, you end up with simpler 2D vectors and rotations can be expressed as simple angles. (Which, when dealing with real 3D math, is never the right formulation, but in 2D planes, simplify everything!)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Calculating Torque
    By jek in forum DYNAMIXEL & Robot Actuators
    Replies: 11
    Last Post: 01-01-2016, 01:00 PM
  2. Calculating frame rate and function time
    By TXBDan in forum Software and Programming
    Replies: 13
    Last Post: 05-22-2013, 04:05 PM
  3. Servo reading position and lock position CW
    By mkanon in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 03-30-2013, 05:10 PM
  4. Question(s) 6 Leg 3DOF Walker Kinematics
    By lunarnexus in forum Humanoids, Walkers & Crawlers
    Replies: 32
    Last Post: 04-12-2008, 03:10 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •