Results 1 to 3 of 3

Thread: BubbleBoy

  1. BubbleBoy

    Hi! This is my emotional robot, BubbleBoy!



    Emotions usually are forgotten when it comes to robotics... but this robot is all about emotions! It has two buttons, one for food and one for water. When pressed, these contribute to BubbleBoy's food and water levels, which then are combined as an average to create the health level.



    The health level is then used to determine the mood that BubbleBoy is in. Its moods range from 'Hypertastic!' to 'Dead'. For all of its moods, it has a specific action set that BubbleBoy uses to try to impress you! So this can include BubbleBoy hula-ringing (the lime hula-ring starts to vibrate), spinning its hat (once, twice, or hypertastically), twitching its head on the x and y axis, or bobbing its head on the x and y axis.



    Since BubbleBoy is incredibly humble in its character, it only accepts food until after it's finished its action set. After about 3 action sets though, BubbleBoy becomes hungry and thirsty. if its thirstiness and hungriness drops to 70 and lower, the pink indicator LED will turn on, so you know you should feed it!



    Although this robot appears to be completely without wires or 'guts', inside of the green box is an Arduino with a ProtoShield, LCD 117 Kit, White on Blue 4 line LCD, and two buttons. Inside of the robot are 2 LEDs, 2 DC motors, 2 servos, and 1 LDR.



    The source code and circuitry can be found here.

    Here's a video of BubbleBoy!

    [ame="http://www.youtube.com/watch?v=7Mp35TkzMUA"]YouTube - BubbleBoy Complete[/ame]
    I hope you like BubbleBoy, even though it's pink, has no wires showing, and is cute


    BubbleBoy wiggles 'Hi!' to you


  2. #2
    Join Date
    Jun 2008
    Location
    CA
    Posts
    61
    Rep Power
    36

    Re: BubbleBoy

    i love this lil guy!

  3. #3
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    106

    Re: BubbleBoy

    Hey RobotGrrl! You snuck under the radar with this entry. I got you entered in this contest

    Nice work btw, very creative!

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Just For Fun CONTEST: Crabfu Challenge = $100
    By crabfu in forum Robotics General Discussion
    Replies: 76
    Last Post: 12-07-2008, 05:02 PM
  2. Project BubbleBoy
    By RobotGrrl in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 04-14-2008, 05:47 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •