Page 1 of 2 12 LastLast
Results 1 to 10 of 14

Thread: Roving Servo Bot

  1. Honorablemention Roving Servo Bot

    My 1st post!

    This is my simple homebrew robot arm mounted on a 3 wheel base. It is made out of aluminium, baseboard and some rc bits and bobs.

    I had to take a crash course in vb.net to code a controller, but having a background in web development (and being a techy nerd) that was not too difficult. I will document the controller interface further down this thred.

    Here is how the bot works (electronically).

    PC (manual or programmed output) -> Bluetooth TX -> Bluetooth RX rs232 adapter -> PIC16F84 - Servos

    Construction.

    Here is the "botboard", it is an 8 channel servo controller using a PIC16F84 running at 20Mz. It allows "position and hold" data for the servos, giving static torque which is perfect for robot arms.



    As I was prototyping it is made out of stripboard. It has connectors for 0-12v, rs232 data in, gnd and +5v (+5v for powring the Bluetooth adapter). Also dual voltage regs for the servo power because when the servos are static they are still powered.

    The PIC is programmed to allow a stream of serial data @ 38400 baud to position the servos in real time.

    From vb I output
    Code:
    serialPort.Write(Chr(ServoNum) & Chr(0 - 240))
    ServoNum = 0-8 then a position 0-240 - 127 being about center.

    One neat thing about the pic code is that it allows the use of "Default position". Within the controller app I can set a desired "start-up" position, send this to the bot and on next powerup it will move the servos to this position.

    That's enough about the bot interface, now the construction of the mechanical hardware.

    1st I had to figure out a good strong lightweight material to use for the arm. I settled on L shaped aluminium bar (B&Q for UK people). It had a natural ledge to allow me to fix a mini servo without using too much glue.



    Here you can see how I mounted the mini servos with double sided tape and tie wraps :-)



    Now for the grabber. For this I designed a simple gear unit that is driven from one servo. The gears rotate in opposite directions. Fixed to the gears are the grab arms.



    These are made from 3mm laminated base board.

    I needed some kind of rubber on the tips of the arms to help grip objects. I found some draught excluder that had double side tape on one side. The draught excluder also acts as a grab cushion :-)



    Here is another shot.



    The base board is the stuff sign makers use for out door signs. It is dirt cheap, easy to cut and supe glue loves it! It is also hardwaring, waterproof and can be sanded. I also used this board to construct a roving base.

    This base needed to provide stability for the arm, contain a power sorce and servos for the wheels.

    Here it is under construction.



    The servos have been modded to provide 360 degrees of rotation. I epoxied round servo horns to a couple of RC plane wheels. You can also see the rs232 port, power switch and battery box. The battery box takes 8 AA batteries and provides balance for the arm.



    Wheel mount detail.

    Now I needed a 3rd wheel. I decided a tail wheel from a rc plane would work best. These have hardware to allow the wheel's shaft to rotae around the Z axis.



    Here you can see the batteries installed and the 3rd wheel setup.

    A slightly blurry show of the bot board in place and connected up.



    Here are a few shots of the arm, it has 6 degrees of freedom. The main servos at the base for rotation and lift are large, whereas the servos at the top of the arm for elbow, wrist, wrist rotation and grab are minis.



    Top of the arm



    Base.



    Here is the Bluetooth -> rs232 adapter mounted and powered.




    Completed! The yellow dots on the wheels are for my testing purposes, they are reference points so I can fine tune the software (no optical encoders of anything flash like that).

    Now for software.



    This has the following features:

    Manual control.
    Slide the siders and the servos move in realtime.

    Program mode.
    This records any movements you made. You can then play these back and the bot will move accordingly.

    Set Default position
    Dumps the current servo positions in EEPROM

    Reset
    Sets the bot to the EEPROM values.

    Load/Save
    Ability to save or load pre-programmed scripts.

    This software is totally coded in vb.net and is configured from a simple set of variables. eg What servo is on channel 1, and what are it's max and min movement values.

    So thats' it, my roving servo bot. I have built identical bases to use on other projects.

    And here is the YouTube Video of the bot in action.



    Enjoy!

  2. #2
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    98

    Re: Roving Servo Bot

    Great little robot. I like the way you creatively used materials, and made it all from scratch.

    Also, great post.

    How much weight can it lift? Does it loose its balance when you lift heavier objects?

    DB

  3. Re: Roving Servo Bot

    Hi,

    It can't lift alot, those little servos are not all that strong. Also the gripper material is only suited for light objects. The weight of those 8 AA's and the fact they are offset to the back should balance out anything with a bit of weight.

  4. #4
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: Roving Servo Bot

    Holy crap Pinter75!

    First off, welcome to the TRC, I'm sure you'll love it here.

    Secondly.... holy crap! Nice work with making your own Servo Controller, AND interfacing it with .NET. I'm with DB too! The creativity with using the materials you used is shear brilliance

    I got you entered in the TRC Project Contest.

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  5. Re: Roving Servo Bot

    Hi Alex,

    Thanks for the welcome :-)

    I am sure I will enjoy it here too, I have plenty more bots to show.

  6. #6
    Join Date
    Apr 2008
    Location
    Nelson, New Zealand
    Posts
    1,356
    Images
    58
    Rep Power
    74

    Re: Roving Servo Bot

    Hey Pinter75, Welcome to this forum, Great project, love your video and how you constructed you arm with the materials you had. Well done.
    People yearn after this robotic dream, but you can't strip your life of all meaning, emotion and feeling and expect to function.


  7. #7
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: Roving Servo Bot

    VERY impressive bot. The construction on it looks incredibly clean. I honestly thought you had a 3D printer for it.

    Scratch built controller, hardware, and software. Major kudos and + rep from me!

  8. #8
    Join Date
    Sep 2008
    Location
    Long Island, NY
    Posts
    41
    Rep Power
    37

    Re: Roving Servo Bot

    Great bot, very well thought out and executed.

  9. #9
    Join Date
    Apr 2008
    Location
    Sunnyvale, CA
    Posts
    378
    Images
    34
    Rep Power
    56

    Re: Roving Servo Bot

    Great bot! I really love the hand-made style, not to mention the outstanding cleverness of the whole design. Excellent work!

  10. Re: Roving Servo Bot

    Howdy,

    I have had access to a laser cutter, so this bot now appears in "smoked" perspex :-)

    This was designed in CorelDRAW! then cut and engraved on a 75Watt laser.

    All parts were painstakingly measured and prototyped in card using my craft robo, before being sent to the laser. It works very well and really looks good!

    Also it has spawned a new project: www.botbuilder.co.uk


Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. RC & Serial Servo Controller Kit
    By Al1970 in forum Garage Sale
    Replies: 0
    Last Post: 01-10-2009, 12:39 AM
  2. Project Explorabot - Roving wireless camera bot.
    By Pinter75 in forum Project Showcase
    Replies: 4
    Last Post: 11-14-2008, 09:40 PM
  3. Question(s) Phidgets and servo voltage
    By Eric in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 05-12-2008, 08:32 AM
  4. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •