Thanks Jes. I'm starting to grasp it all now. So basically, I need to make sure that this relay is capable of outputting enough voltage to the electric strike switch's input in order for the solenoid (tar for the wiki page!) to do it's thing with the magnet and lock?
Maybe this following question would be answered if I read a bit more into it - but because of this solenoid using the magnetic qualities from the way the wires are coiled and the electricity passing through - am I right to assume that for it to be locked there will need to be a constant flow of electricity through it and for the unlocking part just for the relay to simply stop providing voltage? Or, does the strike mechanism somehow lock into place until unlocked??
I suppose I should give an overall better picture of what I'm trying to achieve here. From a recent project at university I have learnt how to interface various fingerprint readers with my C# code. So I am going to literally fit one of Microsoft's fingerprint readers into the neighbouring wall to the door along side two simple LED's (red and green). The computer will be the otherside of the wall which will compare fingerprint images in order to grant access (green LED lit) or deny (red LED lit). In the case of access granted, lock will be opened. Really simple when it comes down to it - and it's only being used at home so I haven't got as many things to take into account as if it were a commercial solution.
Bookmarks