Page 3 of 3 FirstFirst 123
Results 21 to 26 of 26

Thread: Bricked XBee [Sigh]

  1. #21
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Bricked XBee [Sigh]

    Gotcha. I kinda thought that would be the answer to that one.

    Hmm. Decisions...
    I Void Warranties�

  2. #22
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Bricked XBee [Sigh]

    Incidentally: I sent "!!! It's colder than reindeer balls !!!" 15,623 from the Arduino to the PC and "!!! sllab reednier naht redloc s'tI" back from the PC to the Arduino in response. I had one dropped packet, but error recover recovered it, looking at the timestamps in my logs.

    Granted it's only ~75ft, but one is sitting in the kitchen (and I had the microwave running for several minutes which also nukes my Bluetooth anywhere in 30ft) and the other is in the lab, a couple feet from two wireless routers and a bluetooth repeater.

    Something to be said for clean power?
    I Void Warranties�

  3. #23
    Join Date
    Jul 2008
    Location
    South Sphincter Idaho
    Posts
    613
    Images
    104
    Rep Power
    69

    Re: Bricked XBee [Sigh]

    On my front porch it's 4 Deg.F right now...Reindeer got nuthin on us...Bwaaahaaha

    So that's what it looks like in German....
    Team Maggot---Mechs. "Bheka" (retired), "Maggot Mk.3(A)"
    " Keep your stick on the ice ".... Red Green

  4. #24
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: Bricked XBee [Sigh]

    I need to update my answer. Everything was working fine without specifying addresses but it turned out to be slow and I was dropping the occasional packet. I set the destination addresses and saw a massive improvement in performance.

    I also added some recovery stuff to my serial software as well. The robot echos the data stream coming from the computer. If they don't match then the computer resends the data until they do.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  5. #25
    artcar12 Guest

    Re: Bricked XBee [Sigh]

    This worked for me when the reset trick refused to.

    It is possible when using the USB board. You just have to go about it in a different manner.
    1. Take the module out of the interface board.
    2. Connect the interface board to the computer.
    3. Open X-CTU
    4. Go to "Modem Configuration"
    5. Put a check in the "Always update firmware" box
    6. Select proper modem from drop down menu,
    7. Select proper function set and firmware version
    from drop down menus.
    8. Click on the "Write" button. After a few seconds of
    trying to read the modem, you will get an Info box
    that says Action Needed. At this point, CAREFULLY
    insert the module into the interface board.
    9. You may get the info box again a short while after,
    just use the reset button on the interface board.

    This should get you back up and running.

    It can take a couple of tries but it worked for me.

    If you just have a breakout board make sure you hook up the Xbee like this:

    http://www.faludi.com/itp_coursework...e_upgrade.html

    It won't work with just Dout and Din connected. Otherwise follow the instructions above.

  6. #26
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Bricked XBee [Sigh]

    Welcome to the forum, and thanks for that follow-up!
    I Void Warranties�

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Xbee and SSC32
    By Rift in forum Arbotix, Microcontrollers, Arduino
    Replies: 42
    Last Post: 12-15-2008, 12:11 PM
  2. For Sale Xbee Wireless Serial Setup
    By jbod in forum Garage Sale
    Replies: 2
    Last Post: 04-15-2008, 07:29 PM
  3. XBee Question
    By JimH in forum Robotics General Discussion
    Replies: 11
    Last Post: 02-11-2008, 08:45 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •