Page 1 of 2 12 LastLast
Results 1 to 10 of 17

Thread: Adding force sensitive resistors to the phoenix.

  1. #1
    Join Date
    Jul 2008
    Location
    Netherlands
    Posts
    76
    Images
    45
    Rep Power
    44

    Adding force sensitive resistors to the phoenix.

    Hi All,

    Iíve spend some hours of my Christmas vacation in the cold garage. Iíve added LMís FSRís and Iím pretty happy with the result. The rubber cap is just a little bit bigger and all the wires are perfectly hidden in the nylon sleeve.

    I think the pictures will explain it all


    Started with a 8mm aluminium rod and some M3 bolts



    The bumper is a little bit bigger then the FSR but thatís a good good thing because it fits perfectly in the rubber cap.



    The cable is strapped behind the leg so you can hardly see it from the front.



    Here is the endresult:



    The wires are still hanging loose as you can see. Iím making a small circuit to convert the analog signals to digital ones. But I havenít got that ready yet.

    Xan

  2. #2
    Join Date
    Jul 2008
    Location
    Chicago
    Posts
    307
    Rep Power
    48

    Re: Adding force sensitive resistors to the phoenix.

    Im trying to do the same with just a switch. But the problem Im having is debouncing the switch.

    How is the software on this going?

    Paul

  3. #3
    Join Date
    May 2008
    Location
    WNC
    Posts
    413
    Images
    68
    Rep Power
    57

    Re: Adding force sensitive resistors to the phoenix.

    Very cool stuff. The pictures are great as well. Will you be sharing the code on making them work?
    +rep for sharing

  4. #4
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: Adding force sensitive resistors to the phoenix.

    Wow that looks great man. Does the rubber bumpon affect the response of the FSR?
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  5. #5
    Join Date
    Jul 2008
    Location
    Netherlands
    Posts
    76
    Images
    45
    Rep Power
    44

    Re: Adding force sensitive resistors to the phoenix.

    Hi All,

    Thanks for the reactions!

    Quote Originally Posted by Quantum View Post
    Im trying to do the same with just a switch. But the problem Im having is debouncing the switch. How is the software on this going?
    Just a switch should be enough to measure if the feet touches the ground. Canít you add a switch with a spring to return it to the basic position?

    I didnít start on the software part yet. I have to improve some other small parts and get V2.0 up and running before Iím gone include the terrain adaption. But I wanted to get away from my desk for some hours

    Quote Originally Posted by ooops View Post
    Very cool stuff. The pictures are great as well. Will you be sharing the code on making them work? +rep for sharing
    Thanks! Yepp, Iím gone share this code as well. Iím planning to release a major update with release 2.0. There is a lot of speed improvement in there. And Iím gone include the terrain adaption in 2.0 and release it in 2.1. You can check the latest status at my topic on lynxmotion

    Quote Originally Posted by jes1510 View Post
    Wow that looks great man. Does the rubber bumpon affect the response of the FSR?
    I didnít had the time to test the affect of the rubber bumper and the working angle. Iím hoping to get some results later on this week. Lets hope for the best

    Thanks, Xan

  6. #6
    Join Date
    Jul 2008
    Location
    Chicago
    Posts
    307
    Rep Power
    48

    Re: Adding force sensitive resistors to the phoenix.

    Just a switch should be enough to measure if the feet touches the ground. Can’t you add a switch with a spring to return it to the basic position?
    The problem is the switch jumps open to close several times and the leg doesn't stop but studders.

    The software runs to fast for the switch so I have to make circuit like this:
    Values will be different just have to do the math.

    Ill start a thread about this once I got something finished.

    Paul

  7. #7
    Join Date
    Jul 2008
    Location
    Netherlands
    Posts
    76
    Images
    45
    Rep Power
    44

    Re: Adding force sensitive resistors to the phoenix.

    Hi All,

    I had those pictures lying around for a couple of weeks but didnít had time to post them. ops:

    I did some testing with the setup on a breadboard before I found the right resistor value. The value needs to be very precise to let it work. With other values the rubber caps give enough force to prevent the Schmitt trigger from switching. I came out with some 6k8 resistors and they work pretty good.

    Iíve made a home brew PCB with the needed components. I miss the time that I went to school and simply could walk to the lab and made my own ďprofessionalĒ PCBísÖ :roll:


    Any suggestion for a company who can make me a real PCB is welcome.

    The 9V battery for the logic is moved to the upper deck to create some space for the PCB. Everything is connected now and Iím pretty happy with the result!

    The PCB is placed upside-down where you can see the green wires sticking out.

    No update on the programming yet.

    Xan

  8. Re: Adding force sensitive resistors to the phoenix.

    Any suggestion for a company who can make me a real PCB is welcome
    I have been using these guys since December of 2007, and everytime I order a PCB, if I order it in the morning, I get it that afternoon, and this is just FEDEX! Of course I live in the same state, but still. Professional quality, very speedy, very cheap, etc!

    Most of my PCBS are around $15-20

    http://www.procyonpcb.com/

  9. #9
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Adding force sensitive resistors to the phoenix.

    Tybs is hyper-fond of http://www.goldphoenixpcb.biz
    I Void WarrantiesÔŅĹ

  10. #10
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: Adding force sensitive resistors to the phoenix.

    lnxfergy is actually the one who pointed me in their direction. Let's see... $99 for 1000 sq cm, including free shipping. I placed the order on last Friday and its going to be at my doorstep on Monday. That is absolutely outstanding for PCB manufacturing turnaround. Quality is superb (this is the actual company that Sparkfun uses) and you can't beat the price. That said- not a good place to go to for onesie twosie work, but when you consider its usually $15-20 per single board, that adds up quick. I'm getting [25x] 2.5x2.5" boards for $99.

    Quote Originally Posted by Adrenalynn View Post
    Tybs is hyper-fond of http://www.goldphoenixpcb.biz

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry Phoenix, a multilegged creature
    By Zenta in forum Project Showcase
    Replies: 123
    Last Post: 12-24-2010, 02:51 AM
  2. Project Project BlackWido & Phoenix
    By Xan in forum Humanoids, Walkers & Crawlers
    Replies: 18
    Last Post: 10-16-2008, 01:51 AM
  3. Question(s) Force Sensing Resistors
    By BrandonG32 in forum Sensors
    Replies: 4
    Last Post: 06-30-2008, 01:19 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •