Results 1 to 4 of 4

Thread: Yes... Another WALL-E hack

  1. Yes... Another WALL-E hack

    Well, I was going to wait until I had a bit more done on this project before posting anything but I thought I would share the work so far (which isn't much).

    To start off with I thought I'd give you a bit of background on myself. My name is Kirk and I work in IT on a beautiful tropical island off the north-east coast of Australia. I have no experience with robotics but it has always been an area that I have wanted to gain a bit more knowledge in. I think I may be a bit over my head with this project but I find that's the best way to learn. So if you see areas I could improve or may be doing something wrong please let me know. I will have a lot of questions for you!

    I am a fan of WALL-E as I'm sure many people are here and this project was mainly inspired by 4mem8

    My idea was to take a wall-e toy and fit a pico itx inside to give wall-e that bit of extra processing power that he deserves. So... I went and started spending some money.



    Inside, wall-e will have a VIA pico itx using a 16gb CF card on a SATA converter as storage. Originally I bought a 2.5" laptop hdd but found that it was slightly too big once the cables were connected to it. He will also have a lynxmotion ssc-32 board to control his servos.


    It's going to be a tight fit but it will be possible to get everything inside. The pico itx will be powered by a 2S 3300mAh lipo battery and the ssc32 and servos will be powered by a slightly smaller lipo. To save space I'm not going to fit a motor controller but rather run wall-e's tracks from continuous rotation servos from the ssc32. (I hope that's possible)

    The plan is to use roborealm with the pico itx so I pulled wall-e's head apart, fitted a camera in one of his eyes and mounted the eyes to a pan/tilt lynxmotion setup.




    Next steps will be taking my dremel and grinding out as much of the excess plastic inside that I can. I will also need to make a few cuts in the bottom of wall-e to be able to connect the servos to his tracks.

    After I get this running I will start playing around with servos on his arms. I also have a set of lynxmotion little grippers that I'd like to add on.

    I will keep updating with pictures and commentary as I go but if anyone has any comments or suggestions I'd really love to hear them.

  2. #2
    Join Date
    May 2008
    Location
    WNC
    Posts
    413
    Images
    68
    Rep Power
    57

    Re: Yes... Another WALL-E hack

    great start! Keep us posted
    I reject your reality and inject my own.
    www.Trampbot.org

  3. #3
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: Yes... Another WALL-E hack

    Nice work so far!
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  4. #4

    Re: Yes... Another WALL-E hack

    I put a couple of the "Parallax" Futaba continuous rotation servos on an RC tank I hacked for a robot base and they work really well and work with the ssc32. Good luck with Wall-E!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  2. Contest Entry Make a wall avoiding robot! Part 1
    By Brandon121233 in forum Project Showcase
    Replies: 16
    Last Post: 09-12-2007, 04:41 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •