Results 1 to 4 of 4

Thread: Wheels to mount to 1/4" output shaft?

  1. Wheels to mount to 1/4" output shaft?

    I am starting a new robotics project using some surplus motors I bought a while back. The motors have a 1/4" output shaft with a flat. For the life of me, I haven't been able to find a commercially available wheel that will easily attach to this size shaft. I like the banebots wheels, but they do not make a hub to fit a 1/4" shaft. I did find some nylon spacers locally that would bring the diameter up to 1/2". I could then use the Banebots hubs for 1/2" shafts, though I'd been limited to only a few wheel sizes. I was hoping to find something that would attach directly to the output shaft without adapters. Does anyone have any ideas? As far as size of wheel, I'm looking for something between 3 and 5 inches in diameter. The bot will live inside, if that matters. Thanks for your help.

    Ken

  2. #2
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    129

    Re: Wheels to mount to 1/4" output shaft?

    Quote Originally Posted by penquissciguy View Post
    I am starting a new robotics project using some surplus motors I bought a while back. The motors have a 1/4" output shaft with a flat. For the life of me, I haven't been able to find a commercially available wheel that will easily attach to this size shaft. I like the banebots wheels, but they do not make a hub to fit a 1/4" shaft. I did find some nylon spacers locally that would bring the diameter up to 1/2". I could then use the Banebots hubs for 1/2" shafts, though I'd been limited to only a few wheel sizes. I was hoping to find something that would attach directly to the output shaft without adapters. Does anyone have any ideas? As far as size of wheel, I'm looking for something between 3 and 5 inches in diameter. The bot will live inside, if that matters. Thanks for your help.

    Ken
    Check out Servocity.com -- I'm pretty certain they have 1/4" adapters

    -Fergs

  3. Re: Wheels to mount to 1/4" output shaft?

    I found just what I was looking for at servocity. Thanks!

    Ken

  4. #4
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    178

    Re: Wheels to mount to 1/4" output shaft?

    6mm is .236" so well generally fit nice and snug.
    I Void Warranties´┐Ż

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-25-2010, 12:51 AM
  2. Attaching wheels to Hitec 1422 servo
    By gedelen in forum Mechanics / Construction
    Replies: 3
    Last Post: 01-21-2009, 08:34 PM
  3. Colson Wheels to 6mm Shaft
    By Judge in forum Mechanics / Construction
    Replies: 4
    Last Post: 06-06-2008, 09:38 PM
  4. Question(s) fixing Colson wheels on motor shaft
    By stefano.antonelli in forum Mechanics / Construction
    Replies: 6
    Last Post: 02-13-2008, 12:37 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •