Results 1 to 6 of 6

Thread: Flex (bend) sensors: depends on how you bend them...

  1. Flex (bend) sensors: depends on how you bend them...

    Apparently bend sensors read differently on the top vs. the bottom.
    Once bent from the top the readings are more sensitive.
    Anyone know of any that yield the same reading if bent up and down?

  2. Re: Flex (bend) sensors: depends on how you bend them...


  3. #3

    Re: Flex (bend) sensors: depends on how you bend them...

    Don't have any idea of how to make the readings equivalent between "bending in" and bending out". I have some similar sensors, probably the only thing you can do is correct for the readings in software.

  4. Re: Flex (bend) sensors: depends on how you bend them...

    I think it relates to the acetate film they place on the bottom and not the top.
    I have the bi-directional on order, I bet the film is equal on both sides.

  5. #5
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    173

    Re: Flex (bend) sensors: depends on how you bend them...

    I think you'll find that it's the density of carbon. The way they work in short: As the sensor bends the carbon is stretched or compressed. The current passes through the carbon, and as you stretch it out you raise the resistance, and as you compress the carbon you lower it.
    I Void Warranties´┐Ż

  6. Re: Flex (bend) sensors: depends on how you bend them...

    Are you suggesting bending upwards from level is compressing and bending downwards from level is stretching? I would think a bend in either direction from level would generate stretch and raise resistance. However, the only difference is that one side has more plastic laminate than the other. I would argue that the substrate is playing a role in these differences.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  2. Question(s) sensors, sensors, sensors!
    By xx2747 in forum Sensors
    Replies: 8
    Last Post: 11-11-2008, 01:58 PM
  3. help with phidget 8/8/8 and EZ1 sensors
    By rbhutani in forum Arbotix, Microcontrollers, Arduino
    Replies: 18
    Last Post: 07-01-2008, 12:04 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •