Results 1 to 2 of 2

Thread: Components to stock your lap/workshop with

  1. #1
    Join Date
    Mar 2008
    Location
    Knoxville, TN
    Posts
    274
    Images
    35
    Rep Power
    54

    Components to stock your lap/workshop with

    Hey guys, I just want to thank lnxfergy and Jes1510 for helping me put this together. This is a list of what they consider the most common electrical items needed for your workshop or lab. At the top of the list, are 3 very nice kits that come complete with Cabinets, and you can buy the refills for said cabinets later on. All of this was purchased for around $207.17 - I got free shipping because I had a VIP code and spent over $99.00 All parts were purchased from Jameco

    Code:
     
    Jameco Part Number Desc Qty Unit Price Line Price
    81832 COMPONENT KIT,RESISTORS,540 PIECES 1 $31.59  $31.59 
    81867 COMPONENT KIT,CAPS,RADIAL,240 PIECES 1 $36.25  $36.25 
    81859 COMPONENT KIT,CAPS,CERAMIC,520 PIECES 1 $38.45  $38.45 
    68339 HEADER,ST MALE,1RW,36PIN,.1 CTR,.025 PST,.23 GOLD TAIL 10 $0.40  $3.99 
    68574 HEADER,ST MALE,2RW,60PIN,.1 CTR,.025 PST,.23 GOLD TAIL 10 $0.38  $3.84 
    181673 @CONNECTOR,PIN,FEM,SQ POST TINFOR:152733 (10) 50 $0.05  $2.30 
    157383 CONNECTOR,.1 ,1RW,3PIN HSG USE W/100765 & 109575 (10) 20 $0.24  $4.80 
    100812 CONNECTOR,.1 ,1RW,2PIN HSG USE W/100765 (10) 10 $0.23  $2.30 
    100803 CONNECTOR,.1 ,1RW,4PIN HSG USE W/100765 (10) 10 $0.28  $2.80 
    100766 @CONNECTOR,PIN,FEM,POST TIN GOLD PLATE (10) 100 $0.13  $12.70 
    145358 @ CONNCTR,PIN,MALE,SQ.POST TIN USE WITH .100 NONPOL.HSNG (10) 10 $0.15  $1.50 
    308567 HEADER REC,20 CONT,SINGLE ROW, VERTICAL MOUNT 4 $0.75  $3.00 
    1054684 QUAD HALF-H DRIVER/LINEAR, INTERFACE 4 $1.65  $6.60 
    38360 @ TRANS, 2N3904, TO-92, (10), NPN SW HS 200MA 40V 20 $0.07  $1.38 
    35991 @ DIODE,SIL REC,1N4004,1A, 400V PRV (10) 100 $0.03  $2.80 
    38375 @ TRANSISTOR,2N3906,PNP,GP (10) 20 $0.07  $1.32 
    179371 TRANSISTOR,TIP41C,NPN SIL,100Vceo,[email protected],TO-220 10 $0.30  $2.98 
    139580 TRANSISTOR,TIP42C,PNP SIL,100V CEO,[email protected],TO-220 10 $0.31  $3.10 
    23579 IC, LM317T, TO-220, REG VOLT ADJ 1.5A 10 $0.39  $3.90 
    51262 IC, 7805T, TO-220FP, REGULATOR 3PIN 5V 20 $0.32  $6.40 
    51334 IC,7812T 10 $0.32  $3.20 
    107182 IC,LM2940CT-5.0 4 $1.39  $5.56 
    192495 IC,LM2940CT-12 2 $1.49  $2.98 
    23683 IC, LM324N, DIP-14, OP-AMP QUAD LOW POWER 5 $0.28  $1.40 
    49040 IC,7404 4 $1.09  $4.36 
    48979 IC,7400 4 $0.97  $3.88 
    49437 IC,7414 4 $0.69  $2.76 
    24811 IC,DRV/REC.MAX232CPE,5V DIP-16,120KBPS 2 $2.75  $5.50 
    13400 IC,CD4093 10 $0.30  $2.98 
    1708781 2AG OR 5X20MM FUSE CLIP 10 $0.26  $2.55 
    Subtotal:     $207.17

  2. #2
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: Components to stock your lap/workshop with

    I just realized another part we should have thought of: 14pin and 8pin IC sockets.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Interesting littleBits (magnetic electronics components)
    By metaform3d in forum Robot Computers
    Replies: 4
    Last Post: 08-15-2008, 10:05 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •