Results 1 to 2 of 2

Thread: Implementing the Robobuilder wCK servo protocol in a windows DLL

  1. Implementing the Robobuilder wCK servo protocol in a windows DLL

    Hi

    I have been working on a project at robosavvy to implement the several pieces of the robobuilder communications protocol as a DLL.

    I have already implemented the remote control protocol which allowed me to create software to control Robobuilder using a PS2 joystick.
    Video here: http://robosavvy.com/forum/viewtopic.php?t=3271
    Software download here: http://robosavvy.com/forum/viewtopic.php?t=3269



    I am now working on implementing the native wCk protocol in a DLL as well. As you now (or not), the robobuilder controller has a mode where you can talk directly to the servos. It behaves very much like the usb2dynamixel from Robotis except that in this case you don't need the usb2dynamixel. You just connect the controller box to the PC.
    I've posted the preliminary implementation of the protocol/DLL here http://robosavvy.com/forum/viewtopic.php?t=3324

    I would really like to get your feedback and appreciation on this

    Thanks
    Pedro.
    Last edited by PedroR; 02-04-2009 at 10:27 PM.

  2. #2
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    143

    Re: Implementing the Robobuilder wCK servo protocol in a windows DLL

    Wow, great work!

    Thanks a ton! I'll have to check this out when my robot project schedule clears up.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. RC & Serial Servo Controller Kit
    By Al1970 in forum Garage Sale
    Replies: 0
    Last Post: 01-10-2009, 12:39 AM
  2. Question(s) servo and motor controllers
    By csdude in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 06-15-2008, 08:23 PM
  3. Question(s) Phidgets and servo voltage
    By Eric in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 05-12-2008, 08:32 AM
  4. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •