Results 1 to 3 of 3

Thread: What is the difference between a linear servo and a solenoid?

  1. What is the difference between a linear servo and a solenoid?

    "quote"

  2. #2
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    98

    Re: What is the difference between a linear servo and a solenoid?

    A solenoid uses an electromagnet to pull a metal plunger...= All or nothing...some are spring loaded, others use two magnets to push and pull.

    A linear servo uses a threaded "worm" gear to extend or retract...with varying degrees...

    Hope this helps.

  3. #3

    Re: What is the difference between a linear servo and a solenoid?

    A solenoid is more like digital, either "on" or "off", thrust or retract. A linear servo is more analog, many different positions that can be selected through adequate signalling.

    Now of course there can be some overlap between the 2, where a solenoid with spring can be PWMed to a certain position, but a linear servo is probably more accurate in positioning.

    Mechanically, a solenoid is a ferrous piece of material acted upon by a coil producing a magnetic field, moving it from a spring held position to a state of rest between the spring and applied field. Linear servos are typically lead screws driven by motors with position measured by potentiometers or encoders and limit switches.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •