Results 1 to 3 of 3

Thread: Updating RoboBuilder firmware without Windows?

  1. Updating RoboBuilder firmware without Windows?

    RoboBuilder provides a "RBC Upgrade Tool" that lets you download firmware updates (or more interestingly, your own compiled C code) to the RoboBuilder Controller (RBC). But the silly thing only runs under Windows.

    Since the connection to the RBC is just a serial cable, it must be using a bootloader. There must be some simple serial protocol that this bootloader uses to download new code, and if I knew what that protocol was, I could write a cross-platform loader that would work on Mac and Linux (as well as Windows).

    Has anybody already done this? Or, does anyone know anything about ATmega128 bootloaders? Perhaps there is some standard way this is done, such that bootload procedures used in other contexts would work here too. Is anyone equipped to snoop on the data going back and forth between the RBC and the PC when running the RBC Upgrade Tool?

    Thanks,
    - Joe

  2. #2

    Re: Updating RoboBuilder firmware without Windows?

    Hi Joe,

    I has been a while since I looked at this, but check out this:

    http://robosavvy.com/forum/viewtopic.php?t=2686

    Richard

  3. Re: Updating RoboBuilder firmware without Windows?

    Quote Originally Posted by iBot View Post
    I has been a while since I looked at this, but check out this:

    http://robosavvy.com/forum/viewtopic.php?t=2686
    THAT'S IT!!!

    Thanks very much for pointing this out! I'll post any follow-ups to that thread.

    Best,
    - Joe

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Implementing the Robobuilder wCK servo protocol in a windows DLL
    By PedroR in forum Software and Programming
    Replies: 1
    Last Post: 02-04-2009, 10:40 PM
  2. Interesting Robobuilder: Video of controlling Robobuilder with a PS2 gamepad
    By PedroR in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 02-04-2009, 10:30 PM
  3. 25 Years Of Windows
    By srobot in forum Off Topic
    Replies: 29
    Last Post: 01-19-2009, 08:57 PM
  4. programming RoboBuilder in C
    By JoeStrout in forum Humanoids, Walkers & Crawlers
    Replies: 5
    Last Post: 10-30-2008, 09:23 AM
  5. Robobuilder (New Korean Robot Kit)
    By Wingzero01w in forum Humanoids, Walkers & Crawlers
    Replies: 107
    Last Post: 09-26-2008, 06:27 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •