Results 1 to 6 of 6

Thread: beginning build project

  1. Question beginning build project

    hey,

    I'm starting with my first project with DC motors. I want to have the bot be able to travel outside on sidewalk and streets. I'm planning on using 2 wheels and one caster.
    I want to use a chain and sprocket system with the 28.00 banebots motorcontroller.
    I'll be using reinforced plexiglass for a body material.
    I plan on the bot being about 8lbs max. when i'm completely finished.
    Now the only problem i'm having is that i don't know what dc motor to use, but i do know that i want a banebots motor.
    I don't really know how to pick it.
    I expect the robot to travel at walking speed or faster.

    so can anyone give me some advice. I'm using this project as a learning experience so i'd like to learn whatever you have to offer.

    Thank You

    (I'll put a google sketch model up soon.)
    Last edited by jellis359; 03-06-2009 at 05:50 PM.
    you can't say WOW without OW!

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    174

    Re: beginning build project

    >> 28.00 banebots motorcontroller

    You mean two of those controllers - one per motor. And two motors.

    Before you can figure out the motor, you need to figure out the wheels - those directly impact speed and power.
    I Void Warranties�

  3. Question Re: beginning build project

    i want to use an off road 4.75" diameter rc car wheel
    it uses a 6mm shaft
    http://www.trossenrobotics.com/store...5-W-pair-.aspx

    I really have no idea where to start=
    what i'd like:
    -power to push through dirt
    -walking speed
    -chain & sprocket system with shafts and bearing blocks
    -motor controller
    -motor w/ 18Amp max. peak (to work with banebots motor controller)
    -i'd like the bot to be about 1' X 1'

    i was going to use this http://www.trossenrobotics.com/store...385-Motor.aspx with this http://www.trossenrobotics.com/store...l-Bearing.aspx this http://www.trossenrobotics.com/store...-0-8-Wide.aspx this http://www.trossenrobotics.com/store...-Hex-Bore.aspx with steel sprockets and chain for a drive system.

    i want to use a 1/2" thick plexiglass thats 1' by 1' for the body

    i want to use the BS2 and this motorcontroller- http://www.trossenrobotics.com/store...45A-peak-.aspx

    how does it look (what do you suggest/what can you teach)
    Last edited by jellis359; 03-07-2009 at 10:31 PM.
    you can't say WOW without OW!

  4. #4
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    106

    Re: beginning build project

    [moved to rovers forum]

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  5. #5

    Re: beginning build project

    The motor above has a 3/8" output shaft, so different hubs and wheels need to be chosen.
    A very fast walk could be 5 mph, but figure 3 or so for normal people. The motor has a free run of 1000 rpm or so. Estimating running half that speed loaded, 500 rpm on a 4.875 wheel would be about 10 feet per second. The 3 mph walk is about 4.4 feet per second, 5 mph (joggish) around 7.3 feet per second. Some folks go with a rule of not having a robot faster than you are, for safety/liability issues. It might be ok, if you feel confident about control, or it might allow things to get out of hand. If doing RC, it could be controllable. If building autonomous, need to get the long range sensors out, so the robot can detect something before it runs it over.

  6. Wink Re: beginning build project

    how did you calculate this? (for future ref.)
    wait nevermind i remember
    you can't say WOW without OW!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. News/Announcement February 09 WINNERS!
    By DresnerRobotics in forum Project Showcase
    Replies: 9
    Last Post: 02-04-2009, 04:04 PM
  2. News/Announcement Only 1 Week Left to Enter Your Project!
    By DresnerRobotics in forum Project Showcase
    Replies: 9
    Last Post: 12-24-2008, 05:17 AM
  3. News/Announcement August '08 WINNERS!
    By DresnerRobotics in forum Project Showcase
    Replies: 39
    Last Post: 10-09-2008, 12:49 PM
  4. Question(s) has any build the oap robot project
    By robot maker in forum Robotics General Discussion
    Replies: 23
    Last Post: 08-27-2008, 10:47 PM
  5. Ambitious AI / Autonomouns project
    By Marc-X in forum Robotics General Discussion
    Replies: 7
    Last Post: 12-23-2007, 09:24 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •