Page 1 of 2 12 LastLast
Results 1 to 10 of 15

Thread: Xan's Rover with Arm

  1. #1
    Join Date
    Jul 2008
    Location
    Netherlands
    Posts
    76
    Images
    45
    Rep Power
    46

    Xan's Rover with Arm

    Hi All,

    I’ve been working on this project for a couple of weeks now. The project includes a A4WD1 Rover with a AL5B Arm mounted on top. The arm got a total of 6DOF controlled using IK.

    Hardware setup:
    A4WD1 Rover
    AL5B Arm

    Electronics:
    Bot Board 2
    Basic Atom 28 Pro
    Sabertooth
    6V 2800mAh NiMH battery for logic and servos
    12V 1600mAh NiMH battery for the wheels

    I started out by stripping my phoenix code down to a single leg and added the wrist in the IK calculations. The arm IK is calculated in 2D and includes shoulder, elbow and wrist servos. The gripper, wrist rotate and base are directly controlled by the remote. I’ve also tried including the base in the IK to get 3D control but this wasn’t easy to control with a remote.

    There is no SSC used in this project. The 6 servos are driven by a interrupt routine which makes it possible to do group moves and control both positions and speed with the BAP. Because the servos are controlled with the use of interrupts it is possible to drive the servos and do IK calculations at the same time. I used a program from Nathan (AcidTech) as example for the group move. Can’t find the link so I’ll post that later on.

    Time for some pictures!






    The video is showing the current status. [ame=http://www.youtube.com/watch?v=ImNEj4KAIoQ]here[/ame]

    Xan
    Last edited by Xan; 03-18-2009 at 09:54 AM.

  2. #2

    Re: Xan's Rover with Arm

    Pretty fun grabby bot. Any plans to have it detect and grab objects on its own?

  3. #3
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    82

    Re: Xan's Rover with Arm

    Looking good Xan!

    Great work with the kinematics and control (as always ). Are you planning of adding force sensor to the gripper?

    -Zenta

  4. #4
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    54

    Re: Xan's Rover with Arm

    Great looking bot xan. Keep up the good work.

  5. #5
    Join Date
    Jul 2008
    Location
    Netherlands
    Posts
    76
    Images
    45
    Rep Power
    46

    Re: Xan's Rover with Arm

    Hi Guys,

    Thanks for the quick replies! I really appreciate it!

    Quote Originally Posted by robologist View Post
    Pretty fun grabby bot. Any plans to have it detect and grab objects on its own?
    Not yet but it sounds like fun! I’ve got some sensors lying around which should be able to do the job. What should be better to use on this, ultrasonic or GP2D12 IR sensor? I saw Laurent from the LM forum do some crazy stuff with it! I’m not thinking of mounting the sensor on the arm but on the base with maybe a servo to scan horizontal. I might get back on this.

    Quote Originally Posted by Zenta View Post
    Are you planning of adding force sensor to the gripper
    I’ve got some spare FSR’s as well. I think I’ll add this soon because I think this will keep the gripper servo from gripping to hard and overload. Not that it happened but it bends and makes a lot of noise when I stop it to late.

    Quote Originally Posted by sthmck View Post
    Great looking bot xan. Keep up the good work.
    Thanks!

    Xan

  6. #6
    Join Date
    Jul 2008
    Location
    Netherlands
    Posts
    76
    Images
    45
    Rep Power
    46

    Re: Xan's Rover with Arm

    Hi,

    Both you and the guys from TR gave me some good ideas. So I’ve spend most of the weekend adding stuff to my rover.

    I’ve added a FSR to the gripper as described in this tutorial. The gripper now stops when it grabs something so I don’t need to worry if I hold the close button for to long.

    Robologist, You've got it started. You’re question kept me busy this weekend! 8) I’ve added a single servo on the front of the rover. The servo rotates a IR sensor to scan the front for objects. The servo divides the range in 40 steps. It measures the distance with the IR sensor. If the object is wide, it can’t be moved so the rover turns. If the object is narrow enough for the gripper. It tries to move it.

    I’m also planning to add a IR sensor on the gripper to check the height from the object before it throws around my furniture. :P

    With the IR sensor mounted the AL5B wouldn’t give me enough range to grab stuff from the round. I’ve replaced it with the AL5D. The looks massive and it gives me a huge range! 8)

    I've also installed some power plugs to let me charge the batteries without removing the top plate every time.

    Sorry, no pictures yet. I’ll post them soon.

    It’s the first time that I’ve used digital servos. Do they always make so much noise? I’ve also noticed that they start holding there position when power is applied. Is it possible to free the digital servos?

    Xan

  7. #7

    Re: Xan's Rover with Arm

    A rover with one arm is goood ......


    But how about a rover with two arms ..... and legs :P



  8. #8
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    179

    Re: Xan's Rover with Arm

    Ummm, wouldn't that belong in a different thread? Like, I don't know... bipeds?
    I Void Warranties�

  9. #9

    Re: Xan's Rover with Arm

    I have a LM rover under the seat which would make it a hybrid.

    Xan, how long till you get a video up of the sensor in action?

    Sounds great.

  10. #10
    Join Date
    Jul 2008
    Location
    Netherlands
    Posts
    76
    Images
    45
    Rep Power
    46

    Re: Xan's Rover with Arm

    Hi,
    Quote Originally Posted by Orac View Post
    A rover with one arm is goood ......

    But how about a rover with two arms ..... and legs :P
    This is cheating!!
    Great looking bot. Or should I say botS! Nice paint job although the red white and blue in just 3 lines was enough.

    Quote Originally Posted by Orac View Post
    Xan, how long till you get a video up of the sensor in action? Sounds great.
    No date yet, things always take out to be harder then expected. But give me a couple of weeks.

    Here are some new pictures showing the new, bigger AL5D arm on the rover. The pressure sensor and IR with servo are already mounted. I have to wait for some parts to come in to get the IR mounted on top of the gripper. But the wire is already sticking out

    The AL5B didn’t give me enough range to get over the IR sensor. No problem with the D version as you can see 8)







    Here are some close-up photo’s from the sensors.



    Just some pics to compare the heights



    Any comments are welcome!

    Xan

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Fit-Bot - a Fit-PC based rover
    By coppertubing in forum Robot Computers
    Replies: 9
    Last Post: 10-06-2009, 09:32 AM
  2. Project "atron" arm
    By metaform3d in forum Project Showcase
    Replies: 11
    Last Post: 09-30-2008, 09:11 AM
  3. Project Custom joystick to control robot arm
    By HakBot in forum Project Showcase
    Replies: 22
    Last Post: 08-22-2008, 11:44 AM
  4. Replies: 30
    Last Post: 05-29-2008, 11:47 AM
  5. Discussion Rover Kits
    By LinuxGuy in forum Rovers
    Replies: 0
    Last Post: 04-02-2008, 05:48 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •