Trossen Arduino Top Thread
+ Reply to Thread
Page 1 of 7 12345 ... LastLast
Results 1 to 10 of 66

Thread: Meet Squidword

  1. #1
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,585
    Images
    428
    Rep Power
    73

    Meet Squidword

    Squidword is a scratch built robot that has been building up inside me for a while. I was looking for a way to satisfy two needs. One is that I wanted a competent humanoid, and the other was to make a bracket system that I could use pretty much universally for all future walkers. I missed the boat with the humanoid. It was simply too heavy for the class of servos that I had on hand. As for the bracket system, I believe that squidword is testimony to its success.






    I built a stand for Squidword. It really helps out with creating the gates. I didn't think I would have to do any welding when I got into walkers, but I got out old sparky and got to work. The stand is sturdy as heck...So check it out. I'll post the plans on how to make it for anyone interested in making a squidword. Its made using 1 1/4 inch square tube and extruded aluminum.







    There are only a few basic types of bracket in the system. Double servo brackets, single servo brackets, and several types of hinges. Using the bracket system I can make servo brackets for as little as a dollar a pound for aluminum.

    This project submission is three part. I’ve uploaded the PDF files for making this robot, as well as a tutorial on how to build this robot. I'm also working on MAX based software that anyone can use to control a robot using an SSC-32. I've already uploaded the base program. The software I am currently working on expands that so that a person can make a series of walk cycles and store them in the software calling them up later.

    One thing that really excites me about squidword is that he is completely symetrical. I can use that so that by simply assigning the legs different values I can adapt any walk cycle to make him walk in almost any direction.

    I had to make some changes to the software, and it took me a while to solve a couple of problems. The software has a bunch of dials each connected to a servo. You can set the position of the dials, and store them as a part of a sequence. Then you can select a counter which will step through the sequenced poses...creating a gate.
    [ame="http://www.youtube.com/watch?v=-xFH1h0GGp4"]YouTube - Using Mechmover[/ame]

    [ame="http://www.youtube.com/watch?v=kviFk1DT_0k&feature=channel_page"]YouTube - Using Mechmover[/ame]

    [ame="http://www.youtube.com/watch?v=1Nt8DqP9OOo"]http://www.youtube.com/watch?v=1Nt8DqP9OOo[/ame]

    [ame="http://www.youtube.com/watch?v=RPCw1PvO6GE"]http://www.youtube.com/watch?v=RPCw1PvO6GE[/ame]

    [ame="http://www.youtube.com/watch?v=4sDc0knUbCE"]http://www.youtube.com/watch?v=4sDc0knUbCE[/ame]


    Enjoy.

    Tutorial
    Attached Files Attached Files
    Last edited by darkback2; 05-26-2009 at 01:12 AM. Reason: Adding Printable Bracket System -fixed youtube - A

  2. #2
    Join Date
    Jul 2008
    Location
    South Sphincter Idaho
    Posts
    605
    Images
    104
    Rep Power
    46

    Re: Meet Squidword

    Very nicely done..Good job..
    Gary
    Team Maggot---Mechs. "Bheka" (retired), "Maggot Mk.3(A)"
    " Keep your stick on the ice ".... Red Green

  3. #3
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,585
    Images
    428
    Rep Power
    73

    Re: Meet Squidword

    Quote Originally Posted by gdubb2 View Post
    Very nicely done..Good job..
    Gary
    Thanks for the kind words.

    For anyone interested I updated the post and will adding pictures of the stand I made and a youtube video explaining how to use mechmover.

    DB

  4. Trossen Arduino Thread Banner
  5. #4
    Join Date
    May 2008
    Location
    TN
    Posts
    851
    Images
    99
    Rep Power
    52

    Re: Meet Squidword

    Outstanding work man!
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  6. #5
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,585
    Images
    428
    Rep Power
    73

    Re: Meet Squidword

    I updated the first post with a new video.

  7. #6

    Re: Meet Squidword

    nice vid, with no audio, there is a NASTY High pitch squeal. But with mute on its fantastic!

  8. #7
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,585
    Images
    428
    Rep Power
    73

    Re: Meet Squidword

    the high pitched squeel is the sound the digital servos make. Squidword has 4 hs 5990s now which are what are providing the necessary torque to carry around that big lunk of a brain. PC based robotics is great...if you don't mind the weight!

    ok...that was cheezy.

    I'm hoping to have a vid of a live fire test for both squidword and charlie by the end of the week.

    DB

  9. #8

    Re: Meet Squidword

    Ahhh I'm too cheap to buy digital servos

    Still great work!

  10. #9
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,585
    Images
    428
    Rep Power
    73

    Re: Meet Squidword

    I'm like the king of cheap...or was. Basically I was, and still for the ankle servos using MG 995s...Here is the deal though. Half of the MG 995s I got didn't work out of the box. A number of other ones overheated and caught on fire...and the rest, have been troopers. While I agree with you, and find it difficult to justify spending the serious dough people spend on high end servos, I realized that I was spending a lot of money trying to be cheap.

    I settled on this. Every month for the next year or so (next month excluded) I will buy one expensive servo. My family already knows...christmas...my birthday...servos! The set of expensive servos will be what I use to build up squidword, and possibly will be stripped out to build another robot. The point being that I'm not going to spend 2 or 3 grand at once, but instead will relax and realize things like this take time. You could also just start a savings account, and put $100 in a month or so so that at the end of the year you could buy a bunch of servos all at once.

    The second thing is, the digital servos hs 5995s are the only things strong enough to support the weight of the computer without using a lever system.

    Given all of the above, spending $500 or so on 4 of them seamed like a nice compromise. I used cheaper servos for the rest of the robot, and sprung for the good stuff only where I absolutely had to.

  11. #10
    Join Date
    Mar 2008
    Location
    Knoxville, TN
    Posts
    270
    Images
    35
    Rep Power
    33

    Re: Meet Squidword

    Quote Originally Posted by darkback2 View Post
    The second thing is, the digital servos hs 5995s are the only things strong enough to support the weight of the computer without using a lever system.
    He means HS5990's. The 5995's are disco'd and have issues.. They're strong, but, can overheat and die.. No internal shutdown and no heatsink built into the case.. I'm upgrading 4 of my 5995's in my mech to 5990's for this very reason.

    Thanks, Connor

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. Contest Entry Meet Charlie
    By darkback2 in forum Project Showcase
    Replies: 61
    Last Post: 01-29-2012, 12:40 AM
  2. Project Meet CLYDE
    By mannyr7 in forum Project Showcase
    Replies: 68
    Last Post: 04-21-2010, 11:16 AM
  3. Project Meet S.A.M.i
    By ooops in forum Project Showcase
    Replies: 48
    Last Post: 01-16-2009, 09:39 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts