Page 1 of 5 12345 LastLast
Results 1 to 10 of 41

Thread: SSC-32 Controllable linear actuators?

  1. #1

    SSC-32 Controllable linear actuators?

    I was curious if anyone knows of a solution to either making, or buy a completed product that will allow linear actuation through the control of an SSC-32 board.

    I want to use linear actuators to allow 2 arms to move both left and right while simultaneously doing other things.

    I have found one solution at servo city there linear actuators that can be plugged up to any hobby servo control board. The down side is that there a little expensive for me right now $300 a peace and I'm looking for a possible solution to come out a little cheaper. If there even is one.

    Accuracy down to the mm is not totally necessary either.

    Rift

  2. #2
    Join Date
    May 2008
    Location
    TN
    Posts
    853
    Images
    99
    Rep Power
    74

    Re: SSC-32 Controllable linear actuators?

    A microcontroller, H-Bridge, and slid pot might could do what you want if there isn't already an off the shelf solution. I believe Ooops is using a servo driven linear actuator.
    "If A is a success in life, then A equals x plus y plus z. Work is x; y is play; and z is keeping your mouth shut."
    -
    Einstein

    Don't be a HelpVampire

  3. #3
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    98

    Re: SSC-32 Controllable linear actuators?

    As with anything...make it yourself. I've scene pretty cool ones made from 80/20 aluminum, and threaded rod.

    Twist the rod using a continuous rotation servo.

    Chef Omega

  4. #4
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: SSC-32 Controllable linear actuators?

    Have a look at the Firgelli L12 series. I'm running late to a meeting, so I can't go into too much right now, but they seem reasonably priced across the line from what I've seen. You want OPTION I:

    Option I—Integrated controller with industrial and RC servo interfaces
    Wiring:
    1 (green) Current input signal (used for 4–20 mA interface mode)
    2 (blue) Voltage input signal (used for the 0–5V interface mode and PWM interface modes)
    3 (purple) Position Feedback signal(0–3.3 V, linearly proportional to actuator position)
    4 (white) RC input signal (used for RC-servo compatible interface mode)
    5 (red) Motor V+ (+6 Vdc for 6 V models, +12 Vdc for 12 V models)
    6 (black) Ground

    In fact, looks like Trossen did the leg-work already for us on that:

    http://www.trossenrobotics.com/store...-actuator.aspx
    Last edited by Adrenalynn; 01-13-2009 at 02:56 PM.
    I Void Warranties�

  5. #5

    Re: SSC-32 Controllable linear actuators?

    Hrm Adrenalynn while those are indeed nice I'm looking for a bit more distance of travel then those can offer. Unless I'm missing something in the specs.


    Rift

  6. #6
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: SSC-32 Controllable linear actuators?

    And therein lies the rub. We can only scheme solutions to stated problems.
    How about something a little more detailed than "a bit more distance"?
    I Void Warranties�

  7. #7

    Re: SSC-32 Controllable linear actuators?

    haha yeah that would probably help wouldn't it. Around 6-8 inches of travel would be the range.


    Now I know these exist http://www.nookindustries.com/images/nookmodular.jpgand are far beyond what i need,but is there something in that style, which i can control through a servo board. Or is a separate controller going to be the only option?

    The only reason I'm looking to control it though the SSC-32 is for simplicity reasons. I can this way control do all the work through SEQ as opposed to using another set of software for just the actuators.

    Rift

  8. #8
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: SSC-32 Controllable linear actuators?

    I don't see anything for less than $300.

    You know you can control a motor controller from the SSC32, right? Motor controllers talk pwm, ie. they are like servos in the control signals they take.
    I Void Warranties�

  9. #9

    Re: SSC-32 Controllable linear actuators?

    Servocity has some interesting actuators. Not cheap though.

  10. #10

    Re: SSC-32 Controllable linear actuators?

    Adrenalynn do you mean one of these? http://www.lynxmotion.com/Product.as...&CategoryID=10

    How would you go about applying something like this to a linear actuator?

    Would it be something like a rack and pinion setup or something else?


    Rift

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •