Results 1 to 3 of 3

Thread: Wheel position sensor positioning

  1. Wheel position sensor positioning

    I got wheel watchers and I am wondering how important it is to have them exactly centered on the axis of rotation.

    Essentially, I can easily make it fit if it is 1/32" off center. I know if it were a single sensor, it wouldn't matter but this has two sensors that are set up to be the same distance from the center of rotation (I assume) and if its off center, they wont be. What kind of accuracy do I need when setting this up?

    I would like it to be able to measure distance in a straight line with about +/- 2% accuracy and be able to complete a turn of 90 degrees with similar accuracy. I will also be using them to control speed and turning radius in a loop with other sensors.

    Thanks
    Jusitn

  2. #2

    Re: Wheel position sensor positioning

    I believe they include a sensor positioning jig, and do so for a reason. Essentially, if you want them to work, it would be best to adjust the frame they are going into, rather than trying to adjust the position of the encoder disk sensors. 1/32" is probably significantly more than one or 2 strips of the encoder wheel, in addition to causing a variable distance encoded as the wheel turns. This means that the wheel may read an encoder tick to represent 1 mm of travel on one part of the wheels circumference, while being 1.5 mm on another part. If it is able to read the strips at all while off center.

  3. Re: Wheel position sensor positioning

    Yeah, the jig wont work with my setup. I am trying to mod it to fit a setup not driven by servos.

    I am just trying to figure out how accurate I need to get it. Like do I need to get a custom jig made?

    Sense it doesn't seem clear, I will probably try to get it closer than the 1/32" and see how it works. Then if I need to make a jig.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing an educatonal book on robotics
    By darkback2 in forum Robotics General Discussion
    Replies: 107
    Last Post: 05-24-2010, 11:51 PM
  2. Calculate Motor and Wheel Size
    By metaform3d in forum Mechanics / Construction
    Replies: 14
    Last Post: 04-17-2009, 04:24 PM
  3. Question(s) need help with steering for a 3 wheel robot
    By toocool in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 01-24-2009, 01:23 PM
  4. Motor Mount & Wheel Kit with Position Controller
    By ctx32 in forum Robotics General Discussion
    Replies: 7
    Last Post: 08-01-2008, 08:42 PM
  5. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •