Results 1 to 6 of 6

Thread: Usb-uirt

  1. Question Usb-uirt

    A USB-UIRT question.

    I am looking for software to use with my USB-UIRT so I can transfer the commands in my I-Sobot remote to my PC and later transfer the command(s) to my I-Sobot from my PC.
    The USB-UIRT has a Help program that allows only 1 command to be uploaded to the PC and then DL to the robot. I have looked at Girder but this app. seems to be geared to AV & Audio remotes.
    Perhaps I missed something?
    Sugestions anyone?

  2. #2

    Re: Usb-uirt

    Download "Robodance" software. It will control your I-sobot from your pC using your USB-uirt.
    http://www.robodance.com/

  3. #3

    Re: Usb-uirt

    What is a "USB-UIRT"?

    Do you mean UART?

    Is this a language thing?
    Last edited by MikeG; 08-22-2009 at 12:45 AM.

  4. #4
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    177

    Re: Usb-uirt

    "Universal Infra Red Transmitter". I know. Blah. I agree.

    PCMCIA - People Can't Memorize Crummy Industry Acronyms. Seriously, though, it has some acceptance: http://www.usbuirt.com/

    Although the UIRT dates back a fair while before USB, iirc.
    I Void Warranties´┐Ż

  5. #5
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    98

    Re: Usb-uirt

    Hey Guys,

    If I remember correctly there are only a few USB Uirts that work with robodance. Actually I think the lego mindstorms serial tower works, and can be found on ebay sometimes.

    I was goofing around with this a while ago, but I couldn't find the drivers for the transmitter!

    Keep us posted.

    DB

  6. #6

    Re: Usb-uirt

    This is the one I bought. It works perfectly.

    http://www.usbuirt.com/

    I was just using it with my Isobot and Robodance a second ago.

    FYI: Even though the website doesn't list Vista as supported, I haven't encountered any difficulties using the USB-Uirt with Vista. I haven't tried any other IR programs than Robodance, however, so I can't vouch for any other programs working with Vista and USBUIrt.
    Last edited by altwolf; 08-23-2009 at 02:20 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Need recommendation for USB or PCMCIA to RS232 (For AVR or PIC use)
    By nizee in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 03-25-2010, 11:50 AM
  2. Atmel AVR USB Boards
    By Azinman in forum Software and Programming
    Replies: 3
    Last Post: 04-03-2009, 10:48 PM
  3. Need help with usb mini-b connection
    By javafiend in forum Sensors
    Replies: 3
    Last Post: 02-13-2009, 05:09 PM
  4. Question(s) C++, C Serial or USB communications help
    By Eric in forum Software and Programming
    Replies: 5
    Last Post: 10-15-2008, 02:05 PM
  5. Question(s) Installing VCP Driver crashed my USB Ports??
    By Alex in forum Off Topic
    Replies: 30
    Last Post: 07-24-2008, 05:17 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •