Results 1 to 4 of 4

Thread: smallest servos available???

  1. smallest servos available???

    Hey Guys

    I am working on a swarm robotics project and it involves building small quadrapeds but a wanted to know what are the smallest servos available???

  2. #2
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    176

    Re: smallest servos available???

    Do you want the smallest servos, or the smallest servos capable of hoisting at least their own mass?
    I Void Warranties´┐Ż

  3. Re: smallest servos available???

    well more over then small i think I am looking for more of compact servos for a quadruped

  4. #4

    Re: smallest servos available???

    smallest in size servos that I've ran across, are ones for these two sub-micro helicopters:

    http://www.helidirect.com/walkera-se...z24-p-6394.hdx
    http://www.helidirect.com/eflite-rep...mcx-p-8194.hdx

    I don't think there are stats posted for them, but they are non standard. I've used the Walkera ones for my fish: http://www.crabfu.com/swashbot/robot_fish.html and had to switch some wires around to work with the receiver. The mcx servos are even smaller, but are very weak, and linear. They both work off of single cell lipo, so don't think that they can take any more than 3.7v, or handle too much torque. Other than those, there are a huge number micro sized servos that are light and with standard connectors and voltage... such as the ones that I've used for swashbot: http://www.crabfu.com/swashbot/swashbot1.html they are cheap and pretty small. If you look for micro servos for heli or planes, they are typically really small and powerful, such as hs-45b http://www.helidirect.com/hitec-hs45...rvo-p-5242.hdx , which I have used many in my helis and never had issue with. If physical size is your concern then just look up manufacturer stats, they usually tell you size, torque, and voltage.

    I usually get my heli servos from helidirect, they carry a lot of different sizes and types, and range in price quite a bit: http://www.helidirect.com/helicopter...os-c-1_359.hdx

    -Crabfu

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Controlling Servos with a servo controller
    By bodhibuilder in forum Arbotix, Microcontrollers, Arduino
    Replies: 25
    Last Post: 09-29-2008, 12:07 PM
  2. HITEC Servos: Can the OEM RN-1 Servos handle 7.4V?
    By MYKL in forum DYNAMIXEL & Robot Actuators
    Replies: 10
    Last Post: 06-23-2008, 05:39 PM
  3. Easy Programing of servos and play back
    By hotrodled in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 01-30-2008, 04:18 PM
  4. 1HV owner haveing problem with servos, help requested
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 13
    Last Post: 11-08-2007, 02:55 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •