Hi I'm making an automatic lottery wheel for an art project.
It's a wooden wheel about 1 meter diameter and one centimetre thick.
It mounted to a mountain bike rear wheel (gives me the gears and the free wheel for free).
Now I'm going to make this wheel spin for a couple of minutes and then stop for a while and then start to spin again. It will do this for a month straight around the clock.
I'm a software programmer so the coding is not a problem and I have bought this 0/0/4 interface kit from Phidget (http://www.phidgets.com/products.php...roduct_id=1014)
It will do the trick to turn on and off the motor in an interval.
I have bought a motor from Micromotor called E192 (http://www.micromotorssrl.com/motori...riduttori.html). It's a 24 V DC motor. 300Ncm torque. Geared down 246:1. 430 mA (max load).
See documentation: (https://www1.elfa.se/data1/wwwroot/w...A/05445507.pdf)
I can power this from a transformer/adapter plugged in to the wall so no battery is needed.
This is where the easy part ends. I have almost no knowledge of electrics but I'm a good googler. I guess this is not that hard if one knows but it's so basic no-one wants to write a tutorial about it.
What do I need now to power this motor? I have read page after page of info about how to power a dc motor from batteries and making H-Bridges to switch direction... Regulators... capacitors and so on.
But do I really need all this? The wheel is just going to spin in one direction and at a predefined speed. When the motor stops the wheel will keep on turning because of the freewheel in the mountain bike wheel so it will not start to generate current or motorbrake.
Can't I just plug an AC/DC Adapter to the wall and then plug the out-cables into the motor?
What happens if the motor is to weak and it takes some time to get the wheel spinning? Will it melt before I can say... damn? Will it start to burn?
Since I have already built the wheel I know that when it has started to spin it will spin for many minutes without any new force added but its a bit heavy so getting it to spin takes some power (but I think 300Ncm will be enough).
I think it would be good with a fuse. On what current should that burn? 430 mA? Should I use slow or quick burning fuses? I'm a bit worried about current spikes. When the wheel starts to spin, I think, there are higher current than when the wheel is in motion at top speed. Correct?. Is that the 430 mA stated in the documentation as current on max load?
Many questions, I hope you guys can give me some of the answers.
If any information is missing please tell me and I'll try to add it.
Thousands of thanks in advance
Nisse Bergman
Bookmarks