Results 1 to 3 of 3

Thread: linear actuator projects?

  1. linear actuator projects?

    I havent posted in a while because my last project got lost in my curiosity for bipeds. Anyways, I am looking into building a biped that uses linear actuators instead of servos. After searching I keep coming back to either SPAL linear actuators or the servo city ones due to cost, speed and force.

    Spal:

    SPECIFICATIONS
    Stroke 300 mm (11.81")
    Voltage 12 DC
    Push/Pull Ratings
    Dynamic 107 lbs. max
    Static 500 lbs. max
    Extension Speed
    No Load 0.59 in/sec
    Max Load 0.39 in/sec
    Amps
    No Load 0.6
    Full Load 3.4
    Duty 20%
    Enclosure IP54
    Pin Holes 5/16"
    Retracted Length 450 mm (17.72")
    Shaft Dia. 20 mm (0.787")
    Size 18-1/4" x 1-1/2" x 3"
    Shpg. 5 lbs.

    Servo city:

    Operating Voltage: 6.0-12 Volts DC
    Operating Temperature Range: -20 to +60 Degree C
    Operating Speed (12V): 2.00 second at max load
    Dynamic Thrust (12V): 25 lbs. Thrust
    Static Load: 500 lbs.
    Current Drain (12V): 500mah no load operating
    Motor Type: 3 Pole Ferrite
    Potentiometer: I0K
    Gear Type: 4 Metal Gears
    Connector Wire Length: 24"
    Recommended Fuse: 10amp inline
    IP Grade: 2IP 63-total dust protection, water resistant


    I cant seem to find any projects at all utilizing either of these and I was wondering why? Is there something im missing? The spal ones seem to be a little slow and the SC seem on the weak side but does anyone know if these can be theoretically accurate enough to be used in a larger biped? ( I think SC has better speed/force options in the making)

    I think maybe a large arm project using either would be a safe/easier project to learn from to get the electronics etc figured out? Would really like to hear your opinions on these!

  2. #2
    Join Date
    Nov 2007
    Posts
    397
    Images
    71
    Rep Power
    46

    Re: linear actuator projects?

    I know why. The price tag.

  3. Re: linear actuator projects?

    haha The spal ones arent so bad. They can be had for about the cost of higher end servos. ($80 bucks)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. SSC-32 Controllable linear actuators?
    By Rift in forum DYNAMIXEL & Robot Actuators
    Replies: 40
    Last Post: 04-11-2009, 08:03 PM
  2. What is the difference between a linear servo and a solenoid?
    By No0bert in forum Robotics General Discussion
    Replies: 2
    Last Post: 02-20-2009, 09:58 PM
  3. Programming a linear actuator with a USB-1024HLS DAQ
    By aaron.dsouza21 in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 12-29-2008, 07:44 PM
  4. Question(s) Controller for SPAL Linear Actuator
    By Hyper-Blue in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 10-10-2008, 09:38 PM
  5. Whoa, want some linear accuracy?
    By Matt in forum DYNAMIXEL & Robot Actuators
    Replies: 17
    Last Post: 04-15-2008, 02:44 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •