Results 1 to 2 of 2

Thread: semi omnidirectional base

  1. semi omnidirectional base

    Hey earlier I was looking for slip rings so I could make an omnidirectional base, with each wheel able to rotate for directional changes as well as driving. But then I thought There may be a way get get most of the benefits with a much simpler construction. Have 4 wheels, each driven, pointed 45 degress towards the inside of the base. This way it can go foreward,reverse, left and right, and be able to go over obstables less then half the wheels diameter. It could do the whole diangle thing as well, but only on reasonablly flat surgfaces. I could use differential steering to rotate in place. Here is my first attempt at asci art to show you what I am talking about
    / \

    \ /

    thats the idea. I may be able to get away with normal wheels instead of omni. WHat do you think?

  2. #2
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    99

    Re: semi omnidirectional base

    There are several ways to do what you want...for example, using servos to rotate the wheel direction so that wheels can point forward or to the side...one method, or using omnidirectional wheels, probably an easier method. if your looking for ideas check out the rovio and tribot. Both of these use three omnidirectional wheels. I would go for 4...probaby make moving omnidirectionally a bit easier to manage and track.

    Hope this helps.

    DB

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project RSV2 mobile base
    By 4mem8 in forum Rovers
    Replies: 2
    Last Post: 04-25-2008, 04:13 PM
  2. Replies: 0
    Last Post: 03-18-2008, 12:41 PM
  3. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 06:49 PM
  4. Bioloid Tracked Base
    By JonHylands in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 09-12-2007, 11:35 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •