Results 1 to 5 of 5

Thread: Need suggestions for new board

  1. Need suggestions for new board

    Hello Everyone: I need little help regarding the next step I would like to take in robotics. I have approx 40 AX12's, and 3 AX-S1's.
    I'm looking to buy a good board to expand, add additional small servos and if possible be able to use some type GUI for programming. So far, I have taken a look at the Axon and Roboard. Both of these boards require some type of modification in order to get the AX12's running properly. Am I on the right track or is there a board I have overlooked that can meet my requirements? Thanks to however responds.

  2. #2
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    148

    Re: Need suggestions for new board

    The only plug and play controllers out there for the Dynamixels are the CM-5 and the CM-2+, past that any board you use will require some sort of modification. The Roboard only requires that you connect TX/RX on Com 3, and supply the AX-12s with power, but you would have to build a cable to connect them. Not sure what is the deal with the Axon, but since it has a UART I would imaging you would be able to interface the AX-12s without much issue.

  3. Re: Need suggestions for new board

    Ok, so in order to power the AX12's on a Roboard I'm going to need a power source (Rechargeable Batteries) along with some type of power regulator to control the voltage being feed to the Servos. Please correct me if I'm wrong as I learn my way through the Matrix.

  4. #4
    Join Date
    Apr 2008
    Location
    Sacramento, CA, USA Area
    Posts
    5,341
    Rep Power
    183

    Re: Need suggestions for new board

    As long as the power source is not higher than the AX12's can handle (11.1v is great), then no, you don't need a regulator. You'd have a tough time finding one that could handle that many servos anyway.
    I Void Warranties´┐Ż

  5. Re: Need suggestions for new board

    Thanks. Just to be clear I just want to have the most options aval. since I have so many of the AX12's. The most would be about 24 at one time.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Best way: low volt servo on HV board?
    By misfitsailor in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 03-30-2009, 07:28 AM
  2. Interesting PIC GSM Cellular Development Board
    By Matt in forum Robotics General Discussion
    Replies: 3
    Last Post: 02-27-2009, 01:30 PM
  3. Atom based PICO-ITX board as robot brain
    By DAPP in forum Robot Computers
    Replies: 15
    Last Post: 09-05-2008, 10:45 AM
  4. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •